How to Enable Driven Shield

Last modified by Microchip on 2026/03/24 11:29

Information

Note: Driven Shield is applicable only for self capacitance sensors. 

Procedure

For hardware Driven Shield:

Include the required self-capacitance sensors.

In the Configure tab, enable Enable Dedicated Shield Pin and select the corresponding pin from the Select Driven Shield Pin drop-down.

Select Driven Shield Pin

For Driven Shield Plus:

Include the required self-capacitance sensors.

In the Configure tab, enable Enable Driven Shield Plus.

Enabling Driven Shield Plus

Back to Top


For timers-based Driven Shield:

Include the required self-capacitance sensors.

In the Configure tab, enable Enable Dedicated Shield Pin and select the corresponding timer and pin from the Select Dedicated Timer and Select Timer Pin drop-downs. Then click Apply and select Yes

Selecting the corresponding timer and pin

For Driven Shield Plus:

Include the required self-capacitance sensors.

In the configure tab, enable Enable Driven Shield Plus and select the required timer for each pin from the drop-downs. Then click Apply.

Enabling Driven Shield Plus

Back to Top