PIC32MX Modes Of Operation
The PIC32MX Central Processing Unit (CPU) runs at one of the three privilege levels: User, Kernel and Debug. These modes determine the addresses, registers, and instructions that are available to a program.
Kernel Mode
The core enters Kernel mode at reset and when an exception is recognized. While in Kernel mode, the software has access to the entire 4 GB virtual address space, as well as the CP0 registers.
User Mode
User mode access is restricted to the first 2 GB of the address space (0x00000000 through 0x7FFFFFFF) and can be excluded from accessing CP0 functions. Accessing a virtual address above 0x7FFFFFFF in User mode will cause an exception.
Debug Mode
Debug mode is entered on a debug exception. While in Debug mode, the software has access to all Kernel mode addresses and functions, as well as debug segment dseg, which overlays part of the kernel segment KSEG3.
Figure 2-13 (from "Section 2. CPU for Devices with M4K® Core" shows the different memory maps for each mode.

The MIPS32 virtual address space is partitioned into five, traditional, fixed-size segments, kuseg, kseg0, kseg1, kseg2, and kseg3.
kuseg (2GB)
- addresses are cacheable, and accessible in both user-mode and kernel-mode; is designed to be used by user-mode programs
kseg0 (512MB)
- addresses are cacheable, and accessible in kernel-mode only; is designed to be used by kernel-mode programs
kseg1 (512MB)
- addresses are noncacheable, and accessible in kernel-mode only; is designed to be used by kernel-mode programs
- designed for access to peripheral devices and for code that requires noncacheable access, including initialization code
kseg2/3 (1GB total)
- addresses are cacheable, and accessible in kernel-mode only; is designed to be used by kernel-mode programs