PIC32MX Oscillator - System PLL
Contents
The System Phase-Locked Loop (PLL) has a user-selectable input divider, multiplier, and output divider to provide a wide range of output frequencies. The oscillator circuit will consume more current when the PLL is enabled.
System PLL Input Selection

The System PLL can use the Fast RC (FRC) Oscillator or the Primary Oscillator (POSC) as the input. The input is indirectly determined by the System Clock (SYSCLK) setting (FNOSC bits).
On reset, the SYSCLK setting is copied to the Current Oscillator (COSC) setting. COSC determines the input to the PLL.
The input to the System PLL can be changed at run-time but the input divider can not. If you want to change the input to the System PLL at run-time, POSC must be 8 to 10 MHz. This is needed to satisfy the PLL multiplier input requirements (4 to 5 MHz) for both FRC and POSC inputs.
The default input can be configured at program time using #pragma statements and MPLAB® Harmony functions can be used to configure it at run-time.
#pragma config FNOSC = FRCPLL
// Default input is Primary Oscillator with the System PLL
#pragma config FNOSC = PRIPLL
//Run-time configuration using Harmony functions shown below
...
// PLL input is FRC
PLIB_OSC_SysClockSelect(OSC_ID_0, OSC_FRC_WITH_PLL);
// PLL input is POSC
PLIB_OSC_SysClockSelect(OSC_ID_0, OSC_PRIMARY_WITH_PLL);
System PLL Input Divider

The input divider must be chosen such that the resulting frequency applied to the PLL multiplier is between 4 and 5 MHz. The input divider options are as follows:
÷1, ÷2, ÷3, ÷4, ÷5, ÷6, ÷10, ÷12
The default divide value is programmable but it can not be changed at run-time.
#pragma config FPLLIDIV = DIV_1
// default PLL input divider = 12 (max)
#pragma config FPLLIDIV = DIV_12
System PLL Multiplier

The multiplier options are as follows:
x15, x16, x17, x18, x19, x20, x21, x24
#pragma config FPLLMULT = MUL_15
// default PLL multiply = 24
#pragma config FPLLMULT = MUL_24
...
// run-time config sets PLL multiplier to 15
PLIB_OSC_SysPLLMultiplierSelect(OSC_ID_0, 15);
System PLL Output Divider

The System PLL output clock divider options are as follows:
÷1, ÷2, ÷4, ÷8, ÷16, ÷32, ÷64, ÷256
Ensure the output is less than or equal to the maximum device frequency (see specific device datasheet).
#pragma config FPLLODIV = DIV_2
// default PLL output divider = 32
#pragma config FPLLODIV = DIV_32
...
// set PLL output divider to 2
PLIB_OSC_SysPLLOutputDivisorSet(OSC_ID_0, OSC_SYSPLL_OUT_DIV_2);
System PLL Lock Status
The System PLL requires some time to achieve lock when a clock source is first applied. The SLOCK status bit can be checked to determine if enough time has passed to ensure a stable PLL output.
When the clock input to the PLL is changed, the hardware automatically clears this bit. After the PLL start-up timer has expired, the bit is automatically set. Please refer to the specific device datasheet for PLL lock time ("TLOCK" = 2 ms max).
The PLL lock status bit will be set upon the expiration of the timer even if the PLL has not achieved a lock. If the PLL does not stabilize during start-up, SLOCK may neither reflect the status of the PLL lock nor detect when the PLL loses lock during normal operation.
The following MPLAB Harmony function returns the state of the PLL lock status. You are responsible for checking this status anytime you change the input to the System PLL.
bool clockPLL_st;
// function returns value of PLL lock status
clockPLL_st = PLIB_OSC_PLLClockIsLocked(OSC_ID_0);