PIC32MZ Instruction Categories

Last modified by Microchip on 2023/11/09 09:01

CPU Instructions

MIPS32® Release 2 CPU instructions are organized into the following functional groups:

  • Load and Store: Used to load/store operands from memory to/from the General Purpose Register (GPR).
  • Computational: Arithmetic, logic, and shift operations performed on integers represented in two's complement format.
  • Jump and Branch: Instructions that modify the Program Counter (PC).
  • Miscellaneous: Exception handling, conditional move, cache prefetch, NOP.
  • Coprocessor: Instructions that deal with the coprocessor units.

Table 1 provides some example assembly language mnemonics for these categories:

Example assembly language mnemonics

​MIPS32 Release 2 CPU Instructions are fully documented in MIPS® Architecture for Programmers Volume II-A: The MIPS32® Instruction Set Manual.

Back to top

Digital Signal Processor (DSP) Instructions

PIC32 MZ devices with microAptive™ or M5150 Core implement MIPS® DSP ASE Revision 2 instructions. They are classified into the following categories:

  • Arithmetic: Instructions that perform addition/subtraction of Q15/Q31 data.
  • GPR-based Shift: Logical/arithmetic shift operations on DSP data.
  • Multiply/Multiply-Accumulate: MAC operations on DSP data.
  • Bit Manipulation: Specialized DSP bit operations.
  • Compare-Pick: Element-wise comparisons.
  • DSP Control Access: Instructions that access the DSP control register and accumulators.
  • Indexed-Load: Indexed load sub-class.
  • Branch: Specialized branch operation.

Table 2 provides some example assembly language mnemonics for these categories:

Example assembly language mnemonics

​The DSP instruction set is nothing like the regular and orthogonal MIPS32 instruction set. It's a collection of special-case instructions, aimed at known hot spots of important DSP applications.

​MIPS DSP ASE Revision 2 DSP Instructions are fully documented in MIPS® Architecture for Programmers Volume IV-e: The MIPS® DSP Module for the MIPS32® Architecture.

Back to top

Floating Point Unit (FPU) Instructions

PIC32 MZ devices with the M5150 core implement MIPS64® FPU instructions. They are classified into the following categories:

  • Data Transfer: Instructions for moving data to/from the FPU.
  • Arithmetic: Operations on formatted data values.
  • Conversion: These instructions perform conversions between floating point and fixed point data types.
  • Formatted Move: Move formatted operand values among FPU general registers.
  • Conditional Branch: PC-relative conditional branch instructions that test condition codes set by FPU compare instructions.
  • Miscellaneous: Conditionally move one CPU general register to another, based on an FPU condition code.

Table 3 provides some example assembly language mnemonics for these instruction categories:

Example assembly language mnemonics

​For more information on the FPU instruction set, please refer to chapter 12 (50.12) in the PIC32MZ family reference manual Section 50. CPU for Devices with MIPS32® microAptiv™ and M-Class Cores.

Back to top

Macro Instructions

Most MIPS assemblers will synthesize a set of macro (also called synthetic or pseudo) instructions intended to simplify the task of writing MIPS assembly language programs.

Every time a programmer specifies a macro instruction, the assembler replaces it with a set of actual MIPS instructions to accomplish a task.

For example, let us suppose a programmer used the load-immediate (li) macro instruction to load a 32-bit constant into a register:

​1 li     s0, 0x1234AA77

The MIPS assembler would then insert the following two MIPS instructions to accomplish the task:

1 lui     s0, 0x1234
2 ori     s0, 0xAA77
​

Some pseudo-instructions require a temporary register for intermediate calculations. Assemblers use register at for this purpose.

​The mere existence of macro assembly instructions should be a warning sign to budding MIPS assembly language programmers - MIPS machine code might be rather dreary to write!

Visit the MIPS architecture article on Wikipedia for a list of commonly synthesized pseudo-instructions.

Back to top