SAMA7D65 – Dual Boot Feature

Last modified by Microchip on 2026/10/27 04:11

Introduction

In this training, you will learn about the dual boot features of the SAMA7D65 microprocessor (MPU) and you will also learn how to use and test the features. Before learning the dual boot feature, you need to learn how to generate a bootstrap image with a header.

What you will need: 

  • SAMA7D65 Curiosity Kit 
  • Personal computer (Windows®, macOS®, Linux®) running a terminal emulation program
  • USB-to-Serial 3.3 or 5.0 VDC TTL Level adapter with a 6-pin single-in-line 0.1” pitch connector
  • To power the SAMA7D65 Curiosity, you will either: 
    • Connect a USB Type-C® cable to the USB-A port (J3) (included) 
    • Connect an external 5 VDC power supply to DC Jack (J1) 
  • SAM-BA® In-System Programmer (ISP). 

Prerequisites

Ensure the SAM-BA application is added to your $PATH and verify that you have the correct version.

$ sam-ba -v                                                                                                                                     

SAM-BA Command Line Tool v3.9.1
Copyright 2024 Microchip Technology

Back to Top

SAMA7D65 Curiosity Kit

See the "SAMA7D65-Curiosity – Features" page.

Set up the SAMA7D65 Curiosity as listed below to the host computer.

Jumpers

SD Memory Cards

  • Ensure no SD memory card is plugged into the SD card (J4) connector.

Power

Console Serial Communications

Back to Top

How to Generate a Bootstrap Image With a Header

The bootstrap image with header can be generated by two different methods: 1) configuring the at91bootstrap source code using MPLAB X IDE, or 2) using SAM-BA ISP commands. 

In this section, you will generate an at91bootstrap binary image boot.bin with a header from the following commands:

Open a command prompt and change the directory to the location of boot.bin.

<project_directory>\at91bootstrap-4.0.11\build\binaries\boot.bin


Now generate a bootable SAMA7D65 bootstrap image file named "boot_img.bin" with a defined version of 4.25 from a bootstrap binary file named "boot.bin":

$ sam-ba -u gen_image:sama7d65:boot.bin:boot_image.bin:4:25


To view the header information stored in the bootstrap image file, boot_image.bin, use the following command:

$ sam-ba -u parse_image:boot_image.bin

header information

What is Dual Boot?

The Dual Bootstrap feature enables the ROM code to look for a second (secondary) bootstrap, in addition to the first (primary) bootstrap, on the same NVM. This feature is based on the bootstrap version indicated in the bootstrap image header.

When Dual Bootstrap is enabled, the ROM code selects which bootstrap to launch according to the version number. The ROM code launches the bootstrap with the highest version number. If the primary and secondary bootstrap versions are identical, the primary one is launched. If the selected bootstrap is not valid, the ROM code tries to load and launch the other one.

To update the at91bootstrap version number, refer to the "How to Generate a Bootstrap Image With a Header" section.

How to Enable Dual Boot on an SD Card

We can enable dual boot using OTP Emulation mode or using real OTP memory on the SAMA7D65 Curiosity Kit.

Warning: We strongly recommend using the OTP Emulation mode only for testing and prototyping purposes, not for production. In Production mode, the data should be stored and secured in the real OTP memory.

Using OTP Emulation

Remove the SD card and ensure jumper J36 and J39 are removed. Press the RESET (SW4) button. Observe the RomBOOT print on the serial terminal.


Open the command prompt and enter the following command: 

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_ENABLED

This enables emulation mode.


Reset emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c resetemul


Refresh emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:emul


Soft Reset the board.

$ sam-ba -p serial -d sama7d65 -a reset


Enable dual boot by writing the boot configuration packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-emul:FLEXCOM6_USART_IOSET4,SDMMC1_IOSET1_NO_CD_DB@_alt

Using Real OTP Memory

Remove the SD card and ensure that jumpers J36 and J39 are removed.


Press the RESET (SW4) button. Observe the RomBOOT print on the serial terminal.


Disable Emulation mode.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_DISABLED


If a boot configuration packet has already been written to OTP, mark it as invalid.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c invalidatecfg:bcp-otp


Refresh OTP.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:otp


This enables the dual boot feature by writing boot configuration packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-otp:FLEXCOM6_USART_IOSET4,SDMMC1_IOSET1_NO_CD_DB@_alt

How to Implement Dual Boot on an SD Card

Before implementing the dual boot feature, we need to have at91bootstrap images with two different version numbers.

  • Example:
    • One with version number 3.00 (Build time: 2025-07-04 14:38:43) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-07-04 14:21:30) named "boot_alt.bin"
Emulation Mode
Scenario 1: Primary and Secondary bootstrap Versions are Different

Copy both boot.bin and boot_alt.bin into the FAT partition of the SD memory card.


Insert the SD memory card and press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. 

Debug print

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:

    • One with version number 4.00 (Build time: 2025-08-06 14:35:02) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-07-04 14:21:30) named "boot_alt.bin"

Copy both boot.bin and boot_alt.bin into the FAT partition of the SD memory card.


Insert the SD memory card and press the RESET(SW4) button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named boot.bin (Build time: 2025-08-06 14:35:02) will boot.

Boot Success identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid
  • Example:
    • One bootstrap without a version number named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-07-04 14:21:30) named "boot_alt.bin"

Copy boot.bin (without header) from the location  <project_directory>\at91bootstrap-4.0.11\build\binaries\boot.bin (refer to the "SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from SD Memory Card" page) and boot_alt.bin into the FAT partition of the SD memory card.


Insert the SD memory card and press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with valid version number 4.00 will boot.

Debug print

Real OTP Memory
Scenario 1: Primary and Secondary bootstrap Versions are Different

Copy both boot.bin and boot_alt.bin into the FAT partition of the SD memory card.


Insert the SD memory card and press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. 

Debug print

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:
    • One with version number 4.00 (Build time: 2025-08-06 14:35:02) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-07-04 14:21:30) named "boot_alt.bin"

Copy both boot.bin and boot_alt.bin into the FAT partition of SD memory card.


Insert SD memory card and press RESET(SW4) Button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named as boot.bin (Build time: 2025-08-06 14:35:02) will boot. 

Boot Success identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid
  • Example:
    • One bootstrap without a version number named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-07-04 14:21:30) named "boot_alt.bin"

Copy boot.bin (without header) from the location  <project_directory>\at91bootstrap-4.0.11\build\binaries\boot.bin (refer to the "SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from SD Memory Card" page) and boot_alt.bin into the FAT partition of the SD memory card.


Insert the SD memory card and press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with valid version number 4.00 will boot.

Debug print

How to Enable Dual Boot on NAND Flash

We can enable dual boot using OTP emulation mode or using real OTP memory on the SAMA7D65 Curiosity Kit.

Warning: We strongly recommend using OTP Emulation mode only for testing and prototyping purposes, not for production. In Production mode, the data should be stored and secured in the real OTP memory.

Using OTP Emulation

Remove the SD card and ensure jumpers J36 and J39 are removed.


 Press the RESET (SW4) button. Observe the RomBOOT print on the serial terminal.


 Now open command prompt and enter the following command: 

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_ENABLED

This enables emulation mode.


 Reset Emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c resetemul


 Refresh Emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:emul


 Soft Reset the board.

$ sam-ba -p serial -d sama7d65 -a reset


 Now enable dual boot by writing the boot configuration packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-emul:FLEXCOM6_USART_IOSET4,NFC_IOSET1_PMECC0xc2605007_DB@0x20000

Using Real OTP Memory

Remove the SD card and ensure that jumpers J36 and J39 are removed.


Press the RESET (SW4) button. Observe the RomBOOT print on the serial terminal.


Disable Emulation mode.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_DISABLED


If a boot configuration packet has already been written to OTP, invalidate it before proceeding.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c invalidatecfg:bcp-otp


Refresh OTP.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:otp


This enables the dual boot feature by writing boot configuration packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-otp:FLEXCOM6_USART_IOSET4,NFC_IOSET1_PMECC0xc2605007_DB@0x20000

How to Implement Dual Boot on NAND Flash

Before implementing the dual boot feature, we need to have an at91bootstrap image with two different version numbers.

  • Example:
    • One with version number 3.00 (Build time: 2025-08-12 14:52:18) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 14:54:57) named "boot_alt.bin"
Emulation Mode
Scenario 1: Primary and Secondary bootstrap Versions are Different

Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 14:54:57 as highlighted in the image.

Boot Success different

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:
    • One with version number 4.00 (Build time: 2025-08-12 15:47:18) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 14:54:57) named "boot_alt.bin"

Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named "boot.bin" (Build time: 2025-08-12 15:47:18) will boot. Verify the same from the debug prints that the build time is 2025-08-12 15:47:18 as highlighted in the image.

Boot Success identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid

Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with valid version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 14:54:57 as highlighted in the image.

Boot Success different

Real OTP Memory
Scenario 1: Primary and Secondary bootstrap Versions are Different

Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 14:54:57 as highlighted in the image.

Boot Success different

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:
    • One with version number 4.00 (Build time: 2025-08-12 15:47:18) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 14:54:57) named "boot_alt.bin"

Remove jumper J36 (NAND BOOT). Press the RESET (SW4) button.


Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

$ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named "boot.bin" (Build time: 2025-08-12 15:47:18) will boot. Verify the same from the debug prints that the build time is 2025-08-12 15:47:18 as highlighted in the image.

Boot Success identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid

 Remove jumper J36 (NAND BOOT). Press the RESET (SW4) button.


Close jumper J36 (NAND BOOT).


Write the primary bootstrap image file in the NAND Flash memory.

  1. $ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the NAND Flash memory.

  1. $ sam-ba -p serial -d sama7d65 -a nandflash:1:8:0xc2605007 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press RESET(SW4) Button.


Since we have enabled dual boot, the bootstrap image with valid version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 14:54:57 as highlighted in the image.

Boot Success different

How to Enable Dual Boot on QSPI Flash

We can enable dual boot using OTP Emulation mode or using real OTP memory on the SAMA7D65 Curiosity Kit.

Warning: We strongly recommend using OTP Emulation mode only for testing and prototyping purposes, not for production. In Production mode, the data should be stored and secured in the real OTP memory.

Using OTP Emulation

Remove the SD card and ensure that jumpers J36 and J39 are removed.


Press the RESET (SW4) button. Observe the RomBOOT print on the serial terminal.


Now open the command prompt and enter the following command: 

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_ENABLED

This enables emulation mode.


Reset Emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c resetemul


Refresh Emulation.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:emul


Soft Reset the board.

$ sam-ba -p serial -d sama7d65 -a reset


Now enable dual boot by writing the boot configuration packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-emul:FLEXCOM6_USART_IOSET4,QSPI0_IOSET1_DB@0x20000

Using Real OTP Memory

Remove the SD card and ensure that jumpers J36 and J39 are removed. 


Press the RESET (SW4) button Observe the RomBOOT print on the serial terminal.


Disable Emulation mode.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_DISABLED


If a Boot Configuration Packet has already been written to OTP, invalidate the existing packet before proceeding.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c invalidatecfg:bcp-otp


Refresh OTP.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c refreshcfg:otp


This enables the dual boot feature by writing Boot Configuration Packet.

$ sam-ba -p serial -d sama7d65 -a bootconfig -c writecfg:bcp-otp:FLEXCOM6_USART_IOSET4,QSPI0_IOSET1_DB@0x20000

How to Implement Dual Boot on QSPI Flash

Before implementing the dual boot feature, we need to have an at91bootstrap image with two different version numbers.

  • Example:
    • One with version number 3.00 (Build time: 2025-08-12 17:17:35) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 17:22:08) named "boot_alt.bin"
Emulation Mode
Scenario 1: Primary and Secondary bootstrap Versions are Different

Close jumper J39 (QSPI BOOT).


Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 17:22:08 as highlighted in the image.

Boot Success QSPI different

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:
    • One with version number 4.00 (Build time: 2025-08-13 14:53:13) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 17:22:08) named "boot_alt.bin"

Close jumper J39 (QSPI BOOT).


Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR Flash memory.​​​

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named as boot.bin (Build time: 2025-08-13 14:53:13) will boot. Verify the same from the debug prints that the build time is 2025-08-13 14:53:13 as highlighted in the image.

Boot Success QSPI identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid

Close jumper J39 (QSPI BOOT).


Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 17:22:08 as highlighted in the image.

Boot Success QSPI different

Real OTP Memory
Scenario 1: Primary and Secondary bootstrap Versions are Different

Close jumper J39 (QSPI BOOT).


Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 17:22:08 as highlighted in the image.

Boot Success QSPI different

Scenario 2: Primary and Secondary bootstrap Versions are Identical
  • Example:
    • One with version number 4.00 (Build time: 2025-08-13 14:53:13) named "boot.bin"
    • Another with version number 4.00 (Build time: 2025-08-12 17:22:08) named "boot_alt.bin"

Remove jumper J39 (QSPI BOOT). Press the RESET (SW4) button. Close jumper J39 (QSPI BOOT).


 

Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR Flash memory.​​​

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since primary and secondary bootstrap versions are identical, the primary bootstrap image named as boot.bin (Build time: 2025-08-13 14:53:13) will boot. Verify the same from the debug prints that the build time is 2025-08-13 14:53:13 as highlighted in image.
Boot Success QSPI identical

Scenario 3: Primary bootstrap Invalid and Secondary bootstrap Valid

Remove jumper J39 (QSPI BOOT). Press the RESET (SW4) button. Close jumper J39 (QSPI BOOT).


Write the primary bootstrap image file in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c erase -c write:boot.bin -c verify:boot.bin


Write the secondary bootstrap image file at address 0x20000 in the QSPI NOR Flash memory.

$ sam-ba -p serial -d sama7d65 -a qspiflash:0:1:50 -c write:boot_alt.bin:0x20000 -c verify:boot_alt.bin:0x20000


Press the RESET(SW4) button.


Since we have enabled dual boot, the bootstrap image with the higher version number 4.00 will boot. Verify the same from the debug prints that the build time is 2025-08-12 17:22:08 as highlighted in the image.

Boot Success QSPI different

Back to Top

Summary

In this training, you downloaded, configured, and built at91bootstrap using MPLAB X IDE to run on the SAMA7D65 Curiosity Kit. Finally, you cleaned and built the at91bootstrap for production.

Back to Top

What’s Next?

Once the second-stage bootloader, at91bootstrap (boot.bin), has been configured and built, the next step is to configure and build the application (harmony.bin) binary image. The following training topics show how this is done for NAND Flash, NOR Flash (QSPI), and an SD memory card.

Back to Top

Learn More

Back to Top

Collaterals

Back to Top