Sending "Hello World!" from the USART

Last modified by Microchip on 2026/01/09 08:12

In This Video

  • Provide relevant community developed training materials for a useful USART_putstring() function.
  • Modify this to call our USART_Transmit() function.
  • Use delays for testing purposes.
  • Put additional functionality into USART_irq.c and the function prototype to USART_irq.h, so main remains clean.

Procedure

Add Functionality to the USART Program

Add the following function to our program just below the #include statements.

void USART0_Transmit(char* StringPtr){

while(*StringPtr != 0x00){  //Check if there is still more chars to send from the null char
USART_send(*StringPtr);    //Send one char at a time
StringPtr++;}              //Increment the pointer to read the next char

}

Back to Top


Assign a Value to String[]

Add the following line to our main.c above the previous function.

char String[]="Hello world!!";

Back to Top


Call the Function From main.c

Add this line to the main.c file to send the String to the USART.  Place it just below the sie() line.

 USART_putstring(String);

Back to Top


Compile and Run the Program

Open up your terminal program and if you are fast enough, you'll see the following:

Hello World from Terminal

Back to Top


Make it Easier to See in Our Terminal Program

Add a delay function and move the USART_putstring(String) line into our main loop.  We will need to include the delay header file as well.  Here is the new main.c file contents with these changes.

#include <avr/io.h>
#include
<avr/interrupt.h>  //ADDED
#include
"USART_irq.h"
#include
<util/delay.h>

char String[]="Hello world!!";

void USART_putstring(char* StringPtr){

while(*StringPtr != 0x00){  //Check if there is still more chars to send from the null char
USART0_Transmit(*StringPtr);    //Send one char at a time
StringPtr++;}              //Increment the pointer to read the next char

}

int main(void)
{
/* Set the baudrate to 9600 bps using 8MHz internal RC oscillator */
 USART0_Init(MYUBRR);    //CHANGED to PASS MYUBRR from calculation

 sei();
 USART_putstring(String);    

for( ; ; ) {
 /* Echo the received character */
       
       
       
  USART0_Transmit(USART0_Receive());
        USART_putstring(String);
        _delay_ms(1000);
 }
}

Back to Top


Compile and Run the Program

You will see the following in your terminal program.  Every time you click Enter, the terminal program will show what what is being sent from the UART.  Depending on how you set up the terminal program, you might see "Hello world!!" coming in every second as in the video.

Hello World with Delay

Back to Top


Clean up Main Again

Move our new function into the UART_irq.c file. Put the function definition into the USART_irq.h file. Now retest the program to make sure the functionality is still there.

Learn More

Back to Top