How to Implement a Binary Decoder

Last modified by Microchip on 2026/01/09 08:12

Overview

A binary decoder translates the values on n input lines into 2n output lines, making it an essential component in various digital systems such as memory address decoding, seven-segment display drivers, keyboard encoding, and data routing systems to select among multiple lines based on a binary input.

Information

Note: This example demonstrates the implementation of a 2-to-4 decoder, which serves as a foundation for building more complex decoders.

The truth table for a 2-to-4 binary decoder is as follows:

InputsOutputs
ABOUT1OUT2OUT3OUT4
001000
010100
100010
110001

In this table, A and B represent the two input lines, while OUT0, OUT1, OUT2, and OUT3 represent the four output lines. Each output requires an AND gate, and the number of inputs to each AND gate corresponds to the number of input lines in the truth table. For this 2-to-4 decoder example, 4 AND gates, each with 2 inputs, are required.

The diagram demonstrates the implementation of the Boolean expression using the Configurable Logic Block (CLB) module. Typical inputs for a binary decoder include signals from hardware components like switches, GPIO pins, or counters, as well as software-generated signals or clock-driven inputs. These inputs can come from any source that provides binary values for selecting outputs.

MPLAB Melody Binary Decoder Schematic

Requirements

Procedure

Follow these steps to configure the AND gates:

Determine the input conditions for each output

The truth table indicates which input conditions activate each output:

  • A = 0, B = 0: Output OUT0 is activated (set to 1), while the others are deactivated (set to 0).
  • A = 0, B = 1: Output OUT1 is activated.
  • A = 1, B = 0: Output OUT2 is activated.
  • A = 1, B = 1: Output OUT3 is activated.

Convert input conditions into Boolean expressions

From the input conditions, derive the Boolean expression for each AND gate:

  • OUT0 (00): A & B
  • OUT1 (01): A & B
  • OUT2 (10): A & B
  • OUT3 (11): A & B

Back to Top


Implement the CLB Logic

Configure the CLB to implement the 2-to-4 binary decoder circuit. Refer to the block diagram for guidance. This lesson demonstrates a 2-to-4 binary decoder. For decoders with more inputs, n, or different configurations, refer to Step 1 to derive and implement the correct logic for the desired functionality.

Information

Note: If using MPLAB® Code Configurator, use the CLB Synthesizer tool or download the pre-configured CLB file.

Back to Top


Select a Clock Source for the CLB

Any clock source can be used, as the binary decoder operates independently of the clock. The choice of clock will not affect its functionality.

Back to Top


Assign Pins

Connect the decoder's inputs to the desired signal sources (e.g., GPIO pins, software-driven signals, or peripherals), and route the outputs to the appropriate pins or internal connections for further use.

Back to Top


Verify the Design

Use a debugging tool or oscilloscope to confirm that the outputs correctly represent the decoded values based on the input combinations.

Back to Top

Results

The waveform demonstrates the operation of a 2-to-4 binary decoder with two inputs, Input A and Input B, and four outputs: Output 0 to Output 3. Input A toggles at the highest frequency, while Input B toggles at half the frequency. Each output corresponds to a specific combination of the inputs:

  • Output 0 is active when Input B = 0 and Input A = 0.
  • Output 1 is active when Input B = 0 and Input A = 1.
  • Output 2 is active when Input B = 1 and Input A = 0.
  • Output 3 is active when Input B = 1 and Input A = 1.

Only one output is active at a time, confirming the correct behavior of the binary decoder.

Binary Decoder Output Waveform

Back to Top

Learn More

Back to Top