Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
8-bit PIC® MCU Baseline Instruction Set
Last modified by Microchip on 2023/11/09 09:02
This applies to the PIC10F2xx, PIC12C5xx, PIC12F5xx, PIC16C5xx, and PIC16F5xx families.
Information
Notes:
The 9th bit of the program counter will be forced to a ‘0’ by any instruction that writes to the PC except for GOTO (see Section 3.5 “Program Counter” for more on program counter).
When an I/O register is modified as a function of itself (e.g., MOVF PORTB, 1), the value used will be that value present on the pins themselves. For example, if the data latch is ‘1’ for a pin configured as input andis driven low by an external device, the data will be written back with a ‘0’.
The instruction TRIS f, where f = 5, 6 or 7 causes the contents of the W register to be written to the tri-state latches of PORTA, B or C, respectively. A ‘1’ forces the pin to a high-impedance state and disables the output buffers.
If this instruction is executed on the TMR0 register (and, where applicable, d = 1), the prescaler will be cleared (if assigned to TMR0)
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.