dsPIC33A Memory Organization

Last modified by Microchip on 2026/01/09 08:12

Overview

The dsPIC33A contains several distinct memory spaces. The allocation of memory space is controlled by the System Bus Fabric (BMX), which handles redirection of code/data access to the appropriate memory interface, creating a unified, non-overlapping 24-bit addressable (16 MB) memory map.

dsPIC33A Memory

Information

The Bus Matrix also provides support for the CPU to execute instructions from RAM. Refer to the BMX chapter in the device data sheet.

Back to Top

Memory Architecture

The memory space of the dsPIC33A is organized around five major regions:

  • Special Function Register (SFR)
  • X Data RAM (XRAM)
  • Y Data RAM (YRAM)
  • Configuration Register
  • User Program Memory

dsPIC33A Memory Organization v3

Information

Refer to the device data sheet for detailed memory space allocation and address ranges.

Information

The first 64 KB of memory is in Near Memory, meaning these locations may be accessed efficiently using register file instructions that can directly encode the 16-bit address.

Back to Top

SFR Memory

The SFR is split into groups based on the bus speed at which they operate. Infrequent access and initialization SFRs are on the Slow Bus, whereas critical control loop type SFRs are accessed at full speed (relative to the CPU) using the Fast Bus.

SFP Memory Space

Each peripheral bus speed includes an associated peripheral clock, which is provided by the peripheral clock divider:

Peripheral Clock Divider

  • The "Fast Speed" peripheral clock is equal to the CPU or system clock provided by CLKGEN1.
  • The "Standard Speed" peripheral clock is equal to half the CPU clock.
  • The "Slow Speed" peripheral clock is equal to one-quarter the CPU clock.

Back to Top

Peripheral Bus Speed to Peripheral Mapping Example (dsPIC33AK128MC106)

Peripheral Bus Speed Mapping MC106

Information

All Special Function Registers (SFRs) are 32-bits wide.

Back to Top

Data Memory

dsPIC33A devices contain two equal-sized banks of data memory called X RAM and Y RAM. The data memory is accessed using dedicated X and Y Address Generation Units (AGUs) and separate data paths. The BMX handles the redirection of data memory accesses, allowing data memory to be accessed as one linear non-overlapping address range.

Data Memory v2

Data reads and writes for MCU class instructions always access the X and Y data spaces as a single combined data space.

Dual source operand DSP instructions, such as the MAC instruction, access the X and Y data spaces separately to support simultaneous reads for the two source operands.

Information

A new major highlight is the ability to execute instructions from RAM for reduced instruction latency (requiring one additional clock cycle vs cache). This is useful for bootloader applications, which can execute instructions from RAM while performing flash operations. 

Back to Top

Near Data Memory

A 64 KB address space, referred to as near data memory, is reserved in the data memory space between 0x000000 and 0x010000. Near data memory is directly addressable through a 16-bit absolute address field within all file register instructions. The memory regions included in the near data region will depend on the amount of data RAM implemented for each dsPIC33AK device variant.

  • For devices that have smaller amounts of data memory, the near data region can include all of X memory space and possibly some or all of Y memory space.
  • For devices that have larger amounts of data memory, the near data region can include all of X memory space and possibly some or all of Y memory space.

Near Data Memory v2

Back to Top

Configuration Memory

The next region we have is the calibration and configuration region, which is nonvolatile memory.

Configuration Memory v2

It includes a calibration section with a Unified Device ID, as well as a customer One-Time-Programmable Memory (OTP) memory. It also includes registers used for calibration that the user can copy for compensation, such as DAC INL and DNL and op amp compensation.

We then have user configuration pages, UCA1 and UCB. UCA1 contains the configuration bits for the device’s operation. UCB contains the configuration bits for the security features.

Finally, we have user configuration page UCA2 available in dual partition devices.

Back to Top

Program Memory

Finally, we have user program memory beginning at address 0x800000, as well as a movable Interrupt Vector Table (IVT). Program memory is read linearly, like data memory, using the MOV instruction.

Program Memory

Information

Previously, dsPIC33 devices used the Table Read feature to read constants from program memory. In dsPIC33A devices, TBLRDL/TBLRDH features are unimplemented.

Information

For more information on the Flash Program memory module, visit the "dsPIC33A NVM Controller" page.

Back to Top