SAMA5D29-Curiosity – Copy MPLAB® Harmony v3 Application and at91bootstrap to SD Memory Card
Contents
Introduction
In this training topic you will copy two binary images, harmony.bin (an MPLAB® Harmony v3 Software Framework Application) and boot.bin (Second-stage bootloader, at91bootstrap), to a micro Secure Digital (SD) memory card for booting on the SAMA5D29-Curiosity Development Board. Once the images are copied, the micro SD memory card is inserted, and upon reset, the SAMA5D29 will boot and run the application.
For this exercise, you will write the binaries that were created in the training topics:
- SAMA5D29-Curiosity – Getting Started with MPLAB Harmony v3 Development: CSP Application: pio_led_on_off_interrupt
- SAMA5D29-Curiosity – Configure and Build at91bootstrap to Load a MPLAB Harmony v3 Application from SD Memory Card
Prerequisites
- Knowledgeable of the SAMA5D2 Series Boot Process
- SAMA5D29 Data Sheet – Section 17. Standard Boot Strategies
Hardware
For this training, you will use the SAMA5D29-Curiosity Development Board (P/N: EV07R15A).
SAMA5D29-Curiosity Development Board
Setup the SAMA5D29-Curiosity as listed below to the host computer running the SAM-BA® Host Application.
Jumpers
- Set the jumpers to their default positions as shown in the “Jumper Summary” section of the “SAMA5D29-Curiosity - Features” page.
SD Memory Cards
- Ensure no SD memory cards are plugged into SD memory card slots (J6 or J7).
Power
- Apply power as shown in the “Power Options” section on the “SAMA5D29-Curiosity – Features” page.
Secure Digital Multimedia Card (SDMMC)
The SAMA5D29-Curiosity has two SD memory card slots.
- Secure Digital Multimedia Card (SDMMC) (J7) – J7 is an SD or MultiMediaCard (MMC) memory card slot. It is connected to the SD MultiMediaCard port 1 (SDMMC1) peripheral of the SAMA5D29.
- Micro Secure Digital (J6) (Bottom Side) – J6 is a micro SD memory card slot mounted on the bottom side of the development board. It is connected to the SD MultiMediaCard port 0 (SDMMC0) peripheral of the SAMA5D29.
Setup Console Serial Communications
To view the target console, connect the host computer running a terminal emulation program in accordance with the “SAMA5D29-Curiosity – Console Serial Communications” page.
Copy boot.bin to micro SD Memory Card
In this section, you will copy the at91bootstrap binary image, boot.bin, to micro SD memory card.
Change the directory to the location of boot.bin:
<project_directory>\at91bootstrap\build\binaries\
Copy boot.bin to micro SD memory card.
Write harmony.bin to micro SD Memory Card
In this section, you will write the MPLAB Harmony v3 Software Framework application binary image, harmony.bin, to micro SD memory card.
Change the directory to the location of harmony.bin:
C:\Users\<user>\Harmony3\csp_apps_sam_a5d2\apps\pio\pio_led_on_off_interrupt\firmware\sam_a5d2_curiosity.X\dist\sam_a5d2_curiosity\production\
Copy harmony.bin to a micro SD memory card.
Run MPLAB Harmony v3 Application on the Target
In this section, you will insert the micro SD memory card and wake-up the SAMA5D29-Curiosity to run the MPLAB Harmony v3 Software Framework application.
Ensure the QSPI_BOOT (J10) jumper is open.
This will prevent booting from the onboard Serial Quad I/O™ (SQI™) flash memory.
Insert the micro SD memory card into slot J6, located at the bottom of the development board.
Apply power as shown in the “Power Options” section on the “SAMA5D29-Curiosity – Features” page.
The USB-A port (J1) also functions as a source to power the SAMA5D29-Curiosity. The port is limited to 500 mA. If greater current is required, the SAMA5D29-Curiosity should be powered via J2.
To run the application, press the START (SW3) push button to wake up the MPU. It will take a moment for the SAMA5D29 to boot. Observe the RGB LED (D7) lights green (during boot).
Press the USER (SW1) push button and observe the RGB LED (D7) light up green. Release the USER push button and the RGB LED will turn off.

Summary
In this training topic, you copied the binary files harmony.bin and boot.bin to a micro SD memory card for booting on the SAMA5D29-Curiosity and ran the application on the target.
What’s Next?
For training topics on configuring at91boostrap for other Non-Volatile Memories (NVM), see: