SAMA7G54-EK – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from NOR Flash (QSPI) Memory
Introduction
This training topic describes how to download, configure, and build at91bootstrap to load an MPLAB® Harmony v3 Software Framework application binary image (harmony.bin) from NOR Flash (QSPI) Memory to DDR3L SDRAM on the SAMA7G54-EK Evaluation Kit using the MPLAB X Integrated Development Environment (IDE).
Once at91bootstrap has been built, the resulting binary image (boot.bin) can be written to NOR Flash (QSPI) memory using the SAM-BA® In-System Programmer (ISP).
Prerequisites
- MPLAB X IDE installed on the host computer
- MPLAB XC32 Compiler installed on the host computer
Before You Begin
Before you begin configuring at91bootstrap, you will need some information from the production build of the MPLAB Harmony v3 application. In this example, we use harmony.bin as our application image from the "SAMA7G54-EK – Getting Started with MPLAB® Harmony 3 Development: CSP Application: pio_led_on_off_interrupt" training topic.
- NOR Flash Memory offset value to read harmony.bin
- The harmony.bin image size
- The DDR3L SDRAM address to load harmony.bin
These values will be used to configure at91bootstrap in the following steps.
NOR Flash (QSPI) Memory
The SAMA7G54-EK has a 1 Gb octal interface serial NOR Flash memory (U9) (Macronix MX66LM1G45G) configured as 8 bits x 128 MB. It is connected to the Quad Serial Peripheral Interface port 0 (QSPI0) of the SAMA7G54.
Download at91bootstrap
Create a Project Directory
For the purposes of this training topic, we’ll name our project directory at91bootstrap.
Download or clone at91bootstrap version 4
Download or clone from the Linux4sam GitHub repository.
Open Project at91bootstrap
From MPLAB X IDE, select File > Open Project…
An Open Project dialog is displayed.
Find and select the at91bootstrap project directory.
Click on the Open Project button.
The at91bootstrap project will be displayed in the Projects pane (upper left) and the at91bootstrap – Dashboard pane (bottom left).

Configure at91bootstrap Project Properties
Open at91bootstrap Project Properties
Open the at91bootstrap Project Properties using one of the following methods:
- In the Projects pane, highlight at91bootstrap and click on the wrench icon in the at91bootstrap - Dashboard.
- In the Projects pane, right-click on at91bootstrap and select Properties from the menu.
The Projects Properties – at91bootstrap dialog box opens.

Ensure the Device selected is the SAMA7G54.
Configure the XC32 Compiler
In the Categories pane, select Makefile.
Enter the following text in the Build command and Debug build command boxes:
make CROSS_COMPILE="C:/Program Files/Microchip/xc32/v4.30/bin/bin/pic32c-"
Enter the following text in the Clean command box:
make mplabclean CROSS_COMPILE="C:/Program Files/Microchip/xc32/v4.30/bin/bin/pic32c-"

Click on the Apply button.
Configure at91bootstrap to load harmony.bin from NOR Flash (QSPI) Memory
In the Categories pane, select Kconfig and click on the Load button.
Find the at91boostrap project directory and select the configs directory and then select sama7g5ekdf_qspi_uboot_defconfig and click on the Open button.

Make the following changes:
In this step, you are taking an existing default configuration and altering it to load the MPLAB Harmony v3 application (harmony.bin) from NOR Flash (QSPI) memory. This makes configuration a little bit easier than starting from scratch.
Expand Next Software Type and select the Load 4 MB into start of SDRAM radio button.

Expand Demo Application Image Storage Setup
Set Flash Offset for Demo-App to 0x200000
This is the NOR Flash (QSPI) memory offset value to the application binary (here called Demo-App). This value is planned by the developer as part of the memory map of the NOR Flash (QSPI) memory.
Set Demo-App Image Size to 0x400000
This is the image size of the application binary image (here called Demo-App) to be copied from NOR Flash (QSPI) to SDRAM memory by at91bootstrap.
Enter the address to load the application 0x66f00000 to The External Ram Address to Load Demo-App Image.

Click on the Apply and OK buttons.
Build at91bootstrap
Build at91bootstrap
Build the at91bootstrap project using one of the following methods:
- In the Projects pane, right-click on at91bootstrap and select Build from the menu
- Click on the Build icon (hammer) in the tool ribbon.
Observe the build is successful

Note the location of boot.bin:
<project_directory>\at91bootstrap\build\binaries\boot.bin
The boot.bin file is the binary image of at91bootstrap. The boot.bin image can be written to NOR Flash (QSPI) memory using the SAM-BA Host Applet qspiflash. Instructions on how to do this are listed in the What’s Next? section below.
Summary
The at91bootstrap has been configured and built to load an MPLAB Harmony v3 Software Framework application from NOR Flash (QSPI) Memory on the SAMA7G54-EK.
What's Next?