Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Fundamentals of the C Programming Language
Last modified by Microchip on 2025/08/26 05:25
This class provides an introduction to the C programming language (as specified by the ANSI C89 standard) in the context of embedded systems. We cover the C language from the ground up from a non-hardware-specific point of view in order to focus on the various elements of the C language itself. While not required, previous experience with any programming language or experience with microcontrollers would be helpful. The material is accompanied by a series of hands-on exercises designed to reinforce the fundamentals, all of which are conducted within the MPLAB® X Integrated Development Environment (IDE) using the 16-bit C compiler and simulator. Skills learned in this class are applicable to any ANSI C compiler. Hardware and compiler-specific details such as interrupts, memory models and optimization are not discussed. These topics are covered in the compiler-specific classes.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.