C Programming Arrays
Last modified by Microchip on 2025/08/26 05:25
Contents
Arrays:
- May contain any number of elements
- Elements must be of the same type
- The index is zero based
- Array size (number of elements) must be specified at declaration
How to Create an Array
Syntax
type arrayName [size];
- size refers to the number of elements
- size must be a constant integer
Example
1 int a[10]; // An array that can hold 10 integers
2
3 char s[25]; // An array that can hold 25 characters
2
3 char s[25]; // An array that can hold 25 characters
How to Initialize an Array at Declaration
Syntax
type arrayName [size] = {item1, ..., itemn};
The items must all match the type of the array
Example
1 int a[5] = {10, 20, 30, 40, 50};
2
3 char b[5] = {'a', 'b', 'c', 'd', 'e'};
2
3 char b[5] = {'a', 'b', 'c', 'd', 'e'};
How to Use an Array
Arrays are accessed like variables, but with an index:
Syntax
arrayName [index]
- index may be a variable or a constant
- The first element in the array has an index of 0
- C does not provide any bounds checking
Example
1 int i, a[10]; //An array that can hold 10 integers
2
3 for(i = 0; i < 10; i++) {
4 a[i] = 0; //Initialize all array elements to 0
5 }
6 a[4] = 42; //Set fifth element to 42
2
3 for(i = 0; i < 10; i++) {
4 a[i] = 0; //Initialize all array elements to 0
5 }
6 a[4] = 42; //Set fifth element to 42
Creating Multidimensional Arrays
Add additional dimensions to an array declaration:
Syntax
type arrayName [size1]...[sizen];
- Arrays may have any number of dimensions
- Three dimensions tend to be the largest used in common practice
Example
1 int a[10][10]; //10x10 array for 100 integers
2
3 float b[10][10][10]; //10x10x10 array for 1000 floats
2
3 float b[10][10][10]; //10x10x10 array for 1000 floats
Initializing Multidimensional Arrays at Declaration
Syntax
1
2
3
4
5
6
2
3
4
5
6
type arrayName [size0]...[sizen] =
{{item,...,item},
.
.
.
{item,...,item}};
{{item,...,item},
.
.
.
{item,...,item}};
Example
1
2
3
4
5
2
3
4
5
char a[3][3] = {{'X', 'O', 'X'},
{'O', 'O', 'X'},
{'X', 'X', 'O'}};
int b[2][2][2] = {{{0, 1},{2, 3}},{{4, 5},{6, 7}}};
{'O', 'O', 'X'},
{'X', 'X', 'O'}};
int b[2][2][2] = {{{0, 1},{2, 3}},{{4, 5},{6, 7}}};
Visualizing 2-Dimensional Arrays

Visualizing 3-Dimensional Arrays

Array Processing
1 /**************************************************
2 * Print out 0 to 90 in increments of 10
3 **************************************************/
4 int main(void)
5 {
6 int i = 0;
7 int a[10] = {0,1,2,3,4,5,6,7,8,9};
8
9 while (i < 10)
10 {
11 a[i] *= 10;
12 printf("%d\n", a[i]);
13 i++;
14 }
15
16 while (1);
17 }
2 * Print out 0 to 90 in increments of 10
3 **************************************************/
4 int main(void)
5 {
6 int i = 0;
7 int a[10] = {0,1,2,3,4,5,6,7,8,9};
8
9 while (i < 10)
10 {
11 a[i] *= 10;
12 printf("%d\n", a[i]);
13 i++;
14 }
15
16 while (1);
17 }
- Arrays are frequently processed as part of a loop since the same operation needs to be performed on each element
- Operations might include
- Sending strings of characters to or reading strings of characters from a UART
- Performing a mathematical transform on an array of floating point numbers (think digital filters)
- The loop count variable will often be used as the array index itself or in conjunction with the array index