Lab Exercise 15: Arrays of Structures
Objective
This lab introduces you to the syntax used to work with arrays of structures. For this exercise, we have defined a structure to hold the real and imaginary parts of a complex number. You will then need to modify the real and imaginary parts of each element of an array of complex numbers.
Reference Materials
Exercise Files
Procedure
Open the Project
Start MPLAB® X IDE, then click on the Open Project
icon on the main toolbar
Navigate to the folder where you saved the exercise files for this class.
Click on the Lab15.X folder.
Select Open Project
.
Open C Source File
Open the Lab15.c source file from the project tree by double-clicking on its icon.
This will bring up Lab15.c in a window to edit.

Edit the Source File
Multiply the real (re) part of each array element by 10. (HINT: Use *=)
Multiply the imaginary (im) part of each array element by 5 (HINT: Use *=)

Debug Project
Once you finish writing the code:
Click on the Debug Project
button. This will build and send the program to the simulator.
Click on the Continue

button. This begins the simulation. Wait for the UART 1 Output window to finish printing.
Click on the Halt

button. This will stop execution so that we may examine the results.
Verify Results

After successfully building and running your code, you should see the following in the UART1 Output window:
Code Analysis
Line 12-15
This is the type declaration for the complex number structure. There are two members, representing the real (re) and imaginary (im) parts, and the type name is complex.
Line 20
This is a variable declaration. We are creating an array of structures of type complex. The array has three elements, and we are initializing the array as we are declaring it. Note that the syntax we use to initialize the array is essentially the same as initializing a multidimensional array. So, in a more algebraic form, our array now looks like this:
x[0] = 1.1 + j1.2
x[1] = 2.1 + j2.2
x[2] = 3.1 + j3.2
Line 48
Step 3a: At this point, we are now inside the loop, and will be accessing a complex number on each pass. STEP 1 has us multiplying the real part of the current array element by 10. The easiest way to do this is to use the *= operator. The structure member may be accessed by using the dot notation with the array variable and its index:
x[i].re *= 10;
Line 55
We perform a similar operation to step 1, but this time, we will be multiplying the imaginary part by 5:
x[i].im *= 5;
Line 60
This line prints out the recently modified complex numbers in an algebraic format:
printf("%f + j%f\n", x[i].re, x[i].im);
Since the complex number’s members are both floating point types, we need to use %f as our placeholder/formatting characters in the printf() control string. Then, the arguments used are the same as those used on Line 48 and Line 55 to specify a structure member that is part of an array element.
End Debug Session
End the Simulation Session by clicking the Finish Debugger Session
button.
Clear out the UART 1 Output window (Ctrl + L).
Close the Project.
Conclusions
- Arrays of structures allow groups of related structures to be referenced by a common name.
- Individual structures may be referenced by the array index.
- Individual structure members may be referenced by the dot notation, in conjunction with the array name and index.