Lab Exercise 17: Unions
Objective
This lab is designed to help you to understand how to work with unions. The code is very short and performs no practical function, but it will enable you to work with a union variable and observe how it makes use of data memory when values are written to its members.
Note that you will be using the simulator a bit differently this time. Rather than simply running and stopping your code to see the results, you will be setting breakpoints at three points in your code, and stopping at each of them to observe the data in the watch window.
Reference Materials
Exercise Files
Procedure
Open the Project
Start MPLAB X IDE, then click on the Open Project
icon on the main toolbar
Navigate to the folder where you saved the exercise files for this class.
Click on the Lab17.X folder.
Select Open Project 
Open C Source File

Open the Lab17.c source file from the project tree by double-clicking on its icon.
This will bring up Lab17.c in a window to edit.
Edit Source File
Set breakpoints as instructed on lines 73 and 82 by clicking on the line number in the left column.
Edit the code from lines 96 to 104 according to the comments.
Debug Project
Once you finish writing the code:
Click on the Debug Project
button. This will build and send the program to the simulator.
Click on the Continue
button. This begins the simulation which will stop at line 73.Open the Variables window (Shift + Alt + 1) and expand the variables as shown in the accompanying image.

Step Over Code to the Next Breakpoint
Click on the Step Over button
several times.
Observe the changes in the Variable Window after each time an instruction is executed. You should notice when one item is changed all the items in the union are affected.
Results
If your code was correct, then you should have seen the values shown in each of the steps above.
Code Analysis
(NOTE: Line numbers correspond to those in the provided solution file.)
Lines 18-61
This is the union variable declaration for AccumulatorA and AccumulatorB
Line 72
STEP 1: This line assigns a value to the long member of AccumulatorA
Line 82-85
STEP 2: This line assigns a value to the long member of AccumulatorA
Line 96
STEP 3: Creates a variable AccB of type AccumulatorB
Line 98
STEP 3: Clears AccB
End Debug Session
End the Simulation Session by clicking the Finish Debugger Session
button.
Close the Project.
Conclusions
- Unions allow the same memory location to be viewed and manipulated as different data types.
- They make it possible to store different variable types in the same memory location(s).