Messaging Structure
Messaging Structure for Graphics Applications
Summary
This page describes the configuration and usage of the messaging data structure used in Microchip Graphics Applications. Defined in the gfx-gol.h file and typically named Msg by the application, this structure is used to communicate changes in system input to the graphics processing software. The input sources can be:
- A Touch Screen
- An Input Pin or PIC® Special Function Register (SFR)
- Keypad Device
The Microchip-supplied function, TouchGetMsg, will populate Msg when using a touch-enabled display offered as part of a Microchip Development tool. For non-Microchip supported touch displays and for all non-touch input detection, the user's application is responsible for identifying input changes and filling in the Msg data structure.
When an input change has been recorded, the application will fill in Msg and pass it to the GFX_GOL_ObjectMessage function for processing. The sections of this tutorial that cover processing user input and the graphics overview provide the details of how Msg is processed.
Message Structure Definition
Defined in the gfx-gol.h file, the structure of the message is:

Msg can be defined in any file with GFX_GOL_MESSAGE Msg;.
Structure for a Touch-Enabled Display
When populated by TouchGetMsg for a touch-enabled display, Msg will contain:

uiEvent Codes for Touch Displays
| Event Code | Touch Event Detected |
| EVENT_INVALID | Screen was untouched last time and remains untouched |
| EVENT_MOVE | Screen was touched last time, this time the touch is in a different location |
| EVENT_PRESS | Screen was untouched last time and is touched this time |
| EVENT_STILLPRESS | Screen was touched last time and is still touched in the same location |
| EVENT_RELEASE | Screen was touched last time, but is now untouched |
Once filled, Msg is passed on to GFX_GOL_ObjectMessage for processing.
Structure for Pin or SFR Changes

Example of an Analog Pin Change
Expected uiEvent Codes for Analog Pin Changes
| Event Code | Event Detected |
| EVENT_INVALID | Current ADC value is not significantly different from last reported value |
| EVENT_KEYSCAN | Current value of the ADC requires the display to be updated |
| EVENT_CHARCODE | Current value of the ADC requires the display to be updated ( same as EVENT_KEYSCAN) |
Example of a Digital Pin Change
Expected uiEvent Codes for Digital Pin Changes
| Event Code | Event Detected |
| EVENT_PRESS | The Pin value is now High and was Low on previous read |
| EVENT_STILLPRESS | Current and Previous value of the pin is High |
| EVENT_RELEASE | The input value is now Low and was High on previous read |
Structure for Keyboard Input

Example of a Keyboard Input
Expected uiEvent Codes for Keyboard
| Event Code | Event Detected |
| EVENT_KEYSCAN | Value of the Keyscan |
| EVENT_CHARCODE | ASCII code for the keyboard input |