Audio-Tone Generation Using a Lookup Table With MPLAB® Harmony v3: Step 9
Review the Application Code
C LANGUAGE REFRESHER: enumerated types and structures
In case you need it, here is a refresher on enum and struct types.


Application File: app_tone_lookup_table.h
Open file app_tone_lookup_table.h. This file defines application states, data, and APIs.
Application states corresponding to the state machine, described in the "Overview" section above, are shown in the following image:
Observe the application data structure shown in the following image. Notice the variable state. The variable codec is for the data type corresponding to the AK4953 codec.
Observe the CODEC data structure in the following image.
- handle refers to the instance of the opened AK4953 codec driver.
- Buffered Harmony driver APIs (e.g., DRV_I2S_BufferAddWrite) returns a handle for each data buffer submitted for processing (transmission/reception). writeBufHandle holds the buffer handle for the audio data buffers submitted for transmission using the codec API DRV_CODEC_BufferAddWrite.
- The application can register an event handler to notify when the submitted transmission/reception request is completed. bufferHandler holds the address of the function which is called when the audio data buffer has been transferred by the codec driver.
- context holds an application-specific value passed to the driver.
- txbufferObject holds the address of the audio data that needs to be transferred to the codec. In this example, it will hold the address of a sine tone lookup table.
- bufferSize holds the size of the audio data buffer.
Application APIs for initialization, task state machine, and buffer completion events are declared.
Application File: app_tone_lookup_table.c
Open the app_tone_lookup_table.c file. This file defines the tone lookup table and implements the APIs.
The implementation of function APP_TONE_LOOKUP_TABLE_Initialize sets up the default state of tone lookup table task and initializes the variables for the codec driver.
The APP_TONE_LOOKUP_TABLE_Tasks function implements the task’s state machine as shown in the figure in section Overview above. It starts in the APP_TONE_LOOKUP_TABLE_STATE_CODEC_OPEN state and remains in it until it opens the codec driver and gets a valid driver handle.
In state APP_TONE_LOOKUP_TABLE_STATE_CODEC_ADD_BUFFER, the application submits audio data buffers to the driver queue and enters a waiting state (APP_TONE_LOOKUP_TABLE_STATE_CODEC_WAIT_FOR_BUFFER_COMPLETE) for the last submitted buffer to complete. The number of buffers queued is equal to queue size - 1 (i.e., 2 buffers).
The DMA transfers the last buffer and the codec calls the event handler when the buffer transmission is completed. In the event handler APP_TONE_LOOKUP_TABLE_BufferEventHandler, the state of the task is changed from waiting to complete.
A new buffer is submitted from the state APP_TONE_LOOKUP_TABLE_STATE_CODEC_BUFFER_COMPLETE and the state machine goes to the waiting state again.
The cycle of waiting / complete state continues.