Low Power Application on SAM D21 (Arm® Cortex® M0+) MCUs Using MPLAB® Harmony v3 Peripheral Libraries
Objective
This tutorial shows you how to create a low power application on a SAM D21 using MPLAB® Harmony v3 software framework.
The SAM D21 is a 32-bit Arm® Cortex® - M0+ based microcontroller that provides features to reduce power consumption through different Sleep modes, such as Idle and Standby.
- In Idle mode, the CPU is stopped and optionally, some synchronous clock domains are stopped, depending on the IDLE argument. The regulator operates in Normal mode. This mode allows power optimization with a fast wake-up time.
- In Standby mode, all clock sources are stopped, except those which are kept running if requested by a running module or have the ONDEMAND bit set to zero. The regulator operates in Low Power mode. Before entering Standby mode the user must make sure that a significant amount of clocks and peripherals are disabled so that the voltage regulator is not overloaded. This mode allows the device to consume the lowest power with little overhead on wake-up time.
The Power Manager (PM) module is responsible for controlling the Low Power modes. Additionally, the SAM D21 provides SleepWalking. SleepWalking is the capability for a device to temporarily wake up clocks for the peripheral to perform a task without waking up the CPU in STANDBY sleep mode.
The application makes use of the SAM D21 Xplained Pro Evaluation Kit, Power Debugger, and the I/O1 Xplained Pro Extension Kit (sold separately).
The application is developed on the MPLAB Harmony v3 software framework. MPLAB Harmony v3 is a modular framework that provides interoperable firmware libraries for application development on 32-bit MCUs and MPUs. It includes an easy-to-use Graphical User Interface (GUI) (MHC) for selecting, configuring, and generating starter codes, peripheral libraries, and middleware (USB, TCP/IP, Graphics, and so on).
On power-up, the application prints a menu on a PC serial terminal. The menu provides options to measure the device's power consumption in Sleep modes or to measure wake-up time when the device wake-up from one of the Sleep modes. Once the option is selected, the application sets up EIC peripheral clock source and goes to Standby Sleep mode to enable measurement modes.
In this training module,
a. The power consumption of the SAM D21 Xplained Pro board is measured using two tools
- External Power Debugger - A hardware tool
- Data Visualizer - A software tool
The steps to connect and measure the power consumption using these tools are provided in the following sections.
b. Device wake-up time is measured using the Logic Analyzer. The steps to connect and measure the wake-up time are provided in the following sections.
Power Measurement Mode
By default, the application is running with the device in Standby Sleep mode. While the device is in Standby Sleep mode, the user can measure the device's power consumption by following the instructions provided in the following sections.
The device wakes up from Standby mode and enters Active mode when you cover the light sensor (by placing a hand over it, for example) on the I/O1 Xplained Pro Extension kit. Here, you can observe the transition of the device's power consumption from Standby Sleep mode to Active mode on the Data Visualizer tool.
The application prints the room temperature on a serial terminal, and the device goes back to Standby Sleep mode. The LED0 on the SAM D21 Xplained Pro Evaluation Kit is toggled every time the serial console displays the temperature.
When you press the switch button SW0, the application switches from Standby Sleep mode to Idle Sleep mode. Here, you can observe the transition of the device's power consumption from Standby Sleep mode to Active mode and from Active mode to Idle Sleep mode. At this point, you can measure the device's power consumption in Idle Sleep mode by following the instructions provided in the following sections.
The device wakes up from Idle mode and enters Active mode when you cover the light sensor (by placing a hand over it, for example) on the I/O1 Xplained Pro extension kit. Here, you can observe the transition of the device's power consumption from Idle Sleep mode to Active mode on the Data Visualizer tool.
The application prints the room temperature on a serial terminal, and the device goes back to Standby Sleep mode. The LED0 on the SAM D21 Xplained Pro Evaluation Kit is toggled every time the serial console displays the temperature.
Wake-up Time Measurement Mode
By default, the application is running with the device in Standby Sleep mode, and the device wakes up from Standby Sleep mode when you press a switch on the development board.
The application toggles the Wake-up GPIO pin on the device wake-up and then goes to the Idle Sleep mode. You can measure the wake-up time by monitoring the switch SW0 pin and Wake-up GPIO pin on the Logic Analyzer tool.
In the next switch press, you can measure the wake-up time from Idle Sleep mode by monitoring the same switch SW0 pin and Wake-up GPIO pin on the Logic Analyzer tool.
The application switches the device's Sleep mode between Standby Sleep mode and Idle Sleep mode whenever you press the SW0 switch. Therefore, you can measure the wake-up time from these Sleep modes by monitoring the switch SW0 on the Logic Analyzer tool.
Also, the device wakes up from Standby mode or Idle mode when you cover the light sensor by placing your hand over it, prints the wake-up reason message, and goes back to Sleep mode.
The application you create will utilize the following peripherals:
- SERCOM2 (as I²C) peripheral library to read the temperature from the temperature sensor.
- Real-Time Clock (RTC) peripheral library to periodically generate an event for the AC to sample the light sensor.
- SERCOM3 (as Universal Synchronous Asynchronous Receiver Transmitter (USART)) peripheral library to print messages on a serial console running on a computer.
- PORT peripheral library to toggle the LED0.
- Analog Comparator (AC) peripheral library to sample the light sensor analog input and detect whether the light sensor is covered or not.
- PM peripheral library to configure Low Power modes.
- External Interrupt Controller (EIC) peripheral library to control the user button SW0.
- EVSYS peripheral library to trigger the start of the AC conversion on every RTC compare match event. The EVSYS allows for peripheral-to-peripheral communication without CPU intervention. This reduces the burden on the CPU and other resources when compared to conventional interrupt-based systems.
There are Two Approaches to this Tutorial
- Create the project from scratch:
- Use the provided source files and step-by-step instructions below.
- Use the solution project as an example:
- Build the solution project and download it to the SAM D21 Xplained Pro evaluation kit to observe the expected behavior.
Lab Objectives
- Create an MPLAB X IDE Harmony v3 project for a SAM D21 MCU from scratch.
- Use MHC to configure and generate Harmony v3 Peripheral Library code for the RTC, I²C, USART, AC, PM, EIC, EVSYS, and PORT peripherals.
- Use the Harmony v3 Peripheral Library Application Programming Interfaces (APIs) to implement and demonstrate a low-power application.
Resources

Figure: Hardware Setup
Software Tools
- MPLAB® X IDE
- MPLAB X IDE Installation Instructions
- About MPLAB XC32
- MPLAB XC32 Installations Instructions
For this lab, download the following repositories from GitHub:
- CSP: The following table shows the summary of contents.
| Folder | Description |
|---|---|
| apps | Example applications for CSP library components |
| arch | Initialization and starter code templates and data |
| docs | CSP library help documentation |
| peripheral | Peripheral library templates and configuration data |
- DEV_PACKS: The following table shows the summary of contents.
| Folder | Description |
|---|---|
| Microchip | Peripheral register specific definitions |
| arm | Core Specific Register Definitions (CMSIS) |
- MHC: The following table shows the summary of contents.
| File/Folder | Description |
|---|---|
| doc | Help documentation and licenses for libraries used |
| np_templates | New Project templates for supported toolchains |
| *.jar | Java implementations of MHC modules |
| mhc.jar | Main Java executable (run: java -jar mhc.jar -h) |
| runmhc.bat | Windows cmd batch file to run standalone MHC Graphical User Interface (GUI) |
- Use the MPLAB Harmony 3 Content Manager (MHCM) to download the repositories.
Overview
This lab shows you how to create an MPLAB Harmony v3 project from scratch. You will configure and generate Harmony v3 peripheral library code for the RTC, I²C, USART, AC, PM, EIC, EVSYS, and PORT peripherals. It also demonstrates the Low Power mode features of the SAMD21 MCU using light and temperature sensors on the I/O1 Xplained Pro extension kit.

Figure 1. Application Flow sequence
The application flow is as follows:
- On power-up, the application prints the measurement menu and will read the user measurement mode selection.
- If the user selects Power Measurement Mode, the application flow is as mentioned below
- The application keeps the device in Standby Sleep mode. Here, the user can measure the device power consumption in Standby sleep mode on the Data Visualizer tool.
- The RTC is configured as an event generator to generate a periodic (every 500 ms) event to trigger the AC to start conversion.
- The AC acknowledges the event from the RTC and starts the conversion of the light sensor analog signal.
- If the AC comparator output rises above the detect level, then AC produces an interrupt to wake up the CPU.
- In Active mode, the CPU submits an I²C read transfer request to read the temperature value from the temperature sensor on the I/O1 Xplained Pro evaluation kit.
- The application prints the latest temperature value (in a formatted message) on a serial console/terminal using USART.
- The application also monitors the pressing of switch SW0. If a switch press is detected, the application moves the device to Idle Sleep mode. Here the user can measure the device power consumption in Idle sleep mode on the Data Visualizer tool.
- If the user selects Wake-up Measurement Mode, the application flow is as mentioned below
- The application runs in Standby Sleep mode.
- If a switch press is detected, the device will wake up, and the application runs in Idle Sleep Mode. On the next switch press, the application will go into the Standby Sleep Mode. Here, the user can measure the device wake-up time from Standby sleep mode and Idle sleep mode using the Logic Analyzer.
- On every switch press, the application will switch from Standby Sleep mode to Idle Sleep mode and vice-versa.
- In Sleep mode (Standby or Idle), if the user covers the light sensor by placing their hand over it, the device wakes up from the Sleep mode, prints the wake-up reason on the serial terminal, and goes back to the previous Sleep mode.

Figure 2. CPU in Idle or Standby mode
Lab Source Files and Solutions
This ZIP file contains the completed solution project for this lab. It also contains the source files needed to perform the lab by following the step-by-step instructions (see the "Procedure" section on this page).
Extracting the ZIP file creates the following folders:
- samd21_low_power contains the lab solution (in the firmware folder) and source files (in the dev_files folder).
- dev_files contains subfolder sam_d21_xpro which contains application source files and other support files (if any) required to perform the lab (see "Procedure" section below).
- firmware contains the completed lab solution project. It can be directly built and downloaded on the hardware to observe expected behavior.
Procedure
Lab Index
Step 1: Create Project and Configure the SAM D21
- Step 1.1 - Verify Whether MHC Plug-in is Installed in MPLAB X IDE
- Step 1.2 - Create MPLAB Harmony v3 Project Using MPLAB X IDE
- Step 1.3 - Configure Clock Settings
Step 2: Configure I²C, USART, and RTC Peripheral Libraries
- Step 2.1 - Configure RTC Peripheral Library
- Step 2.2 - Configure I²C Peripheral Library, I²C Pins, and Verify I²C Clock
- Step 2.3 - Configure USART Peripheral Library, USART Pins, and Verify USART Clock
Step 3: Configure AC, Event System, and EIC Peripheral Libraries
- Step 3.1 - Configure Analog Comparator (AC) Peripheral Library (PLIB)
- Step 3.2 - Configure External Interrupt Controller (EIC) PLIB for Switch Button, and Configure EIC Clock
- Step 3.3 - Configure Event System (EVSYS) PLIB
Step 4: Configure PM and NVMCTRL Peripheral libraries, LED and Wake-up Test Pins
- Step 4.1 - Configure Power Manager (PM) Peripheral Library
- Step 4.2 - Configure NVMCTRL Peripheral Library
- Step 4.3 - Configure LED and Wake-up Test Pins
- Step 4.4 - Rename the Default Main File
Step 5: Generate Code
Step 6: Add Application Code to the Project
Step 7: Build, Program, and Observe the Outputs