Low Power Application on SAM E54 Using Harmony v3 Peripheral Libraries: Step 1
Verify Whether the MPLAB® Harmony Configurator (MHC) Plugin is Installed in MPLAB X IDE
• Launch MPLAB X IDE from the Microsoft® Windows® Start menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB Harmony 3 Configurator in the menu.

If you don't see it in the menu, install MHC.
Set Up MHC Plugin Window to Open in Standalone Mode
Go to Tools > Options. You will see the Options window open.


Go to Plugins > Window Manager and select Standalone mode. Click Apply and then click OK.

Create MPLAB Harmony v3 Project Using MPLAB X IDE
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MPLAB Harmony 3 Project, then click Next.

Browse to the folder you downloaded the framework to in the Framework Path edit box. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.

In the Project Settings window, apply the following settings:
Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: <Your_folder>\dev\same54_low_power.
Folder: Indicates the name of the MPLABX .X folder. Enter "sam_e54_xpro" to create a sam_e54_xpro.X folder.
Name: Indicates the name of the project that will be shown in MPLAB X IDE. Enter "low_power_sam_e54_xpro" to set the project's name.
Click Next to proceed to Configuration Settings.


Follow the steps below to set the project’s Configuration Settings.
Name: Enter the configuration name as "sam_e54_xpro".
Target Device: Select ATSAME54P20A as the target device.
After selecting the target device, click Finish to launch the MHC.

Click Launch to launch the MHC tool with the selected packages.

The MHC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right click on the project name low_power_sam_e54_xpro and go to Properties.

Make sure that XC32 (v2.41) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Configure Clock Settings

A new window, Clock Easy View, is opened inside MHC.
The Clock Easy View window will then appear on your screen.

Enable the XOSC CTRL 1 and configure the Oscillator input to 12 MHz.

Set XOSC1 as GCLK Generator 0 source.

Set OSCULP32K as GCLK Generator 1 source.

Set XOSC1 as GCLK Generator 2 source and set divisor value as 12.

Disable the DFLL and FDPLL.