Low Power Application on SAMC2x Using MPLAB® Harmony v3 Peripheral Libraries: Step 2
Configure RTC Peripheral Library
Under the bottom left tab, in Available Components, expand Peripherals > RTC.
Double-click, or drag and drop, RTC to add the RTC peripheral library (PLIB) to the project graph. Verify that the RTC clock is set to run at 1 kHz internal ultra-low-power clock.
When a module is added to the project graph, MHC automatically enables the clock to the module. The default RTC clock source is an internal 1 kHz ultra-low-power clock (OSCULP1K).
Go back to the project graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.
Configure I²C Peripheral Library and I²C pins
Under the Available Components tab, expand Peripherals > SERCOM double-click on SERCOM2 or drag and drop to add the SERCOM instance 2 to the project.
Select the SERCOM 2 peripheral library and configure it for I²C protocol as shown.

Open the Pin Configuration tabs by clicking MHC > Tools > Pin Configuration.

Select the MHC Pin Settings tab and sort the entries by Port names as shown below.

Now, select the MHC Pin Table tab and then scroll down to the SERCOM2 module as shown below.
- Enable I²C Clock (I2C SCL) on PA13 (Pin #30)
- Enable I²C Data ( I2C SDA) on PA12 (Pin #29)
Configure USART Peripheral Library and USART pins
Under the Available Components tab, expand Peripheral > SERCOM. Double-click on SERCOM4, or drag and drop, to add the SERCOM instance 4 to the project.
Select the SERCOM 4 peripheral library in the Project Graph and configure it for USART protocol as shown below
Verify the default baud rate is set to 115200 Hz.
Select the Pin Table tab and then scroll down to the SERCOM4 module as shown below.
- Enable USART_TX on PB10 (Pin #23) and USART_RX on PB11 (Pin #24).

Configure DMA Peripheral Library
Launch DMA Configurator by going to the MHC tab in MPLAB® X IDE and then selecting Tools > DMA Configuration.
Click on the DMA Settings tab. Configure DMA Channel 0 to transfer application buffer to the USART TX register. The DMA transfers one byte from the user buffer to USART transmit buffer on each trigger.Based on the trigger source, the DMA channel configuration is automatically set by MHC.
- Trigger Action: Action taken by DMA on receiving a trigger.
- One beat transfer: Generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- One block transfer: Generally used during the memory-to-memory transfer on a software trigger.
- Source Address Mode, Destination Address Mode: Select whether to increment Source/Destination Address after every transfer. Automatically set by MHC based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented, and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed, and the Destination Address is incremented.
- Beat Size: Size of one beat. The default value is 8-bits. For example:
- If the SPI peripheral is configured for 16-bit/32-bit mode, then the beat size must be set to 16-bits/32-bits respectively.

Disable USART interrupt:
Under the Project Graph tab, click on the SERCOM4 block.
In the Configuration Options, uncheck the Enable Interrupts option.