Low Power Application on SAM L21 Using MPLAB® Harmony v3 Peripheral Libraries: Step 1
Create Project and Configure the SAM L21
Verify MPLAB® Harmony Configurator (MHC) Plugin is Installed in MPLAB X IDE
Verify that MHC is installed.
• Launch MPLAB X IDE from the Microsoft Windows® Start menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB Harmony 3 Configurator in the menu.

If you don't see it in the menu, install MHC.
Setup MHC Plugin Window to Open in Standalone Mode
Go to Tools > Options in the MPLAB X IDE toolbar:
Go to Plugins > Window Manager and select Standalone mode. Click Apply and then click OK:
Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog box, select Microchip Embedded. In the Projects pane, select 32-bit MPLAB Harmony 3 Project, then click Next.
In the Framework Path edit box, browse to the folder you downloaded the framework to. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.
In the Project Settings window, apply the following settings:
Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, <Your_folder>\dev\saml21_low_power.
- Folder: Indicates the name of the MPLABX .X folder. Enter "sam_l21_xpro" to create a sam_l21_xpro.X folder.
- Name: Indicates the name of the project that will be shown in the MPLAB X IDE. Enter "low_power_sam_l21_xpro" to set the project's name.
- Click Next to proceed to Configuration Settings.
Follow the steps below to set the project’s Configuration Settings.
Name: Enter the configuration name as "sam_l21_xpro".
- Target Device: Select ATSAML21J18B as the target device.
- After selecting the target device, click Finish to launch MHC.
Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in the MPLAB X IDE. Right click on the project name "low_power_sam_l21_xpro" and go to Properties.
Make sure that XC32 (v2.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.
Launch MHC from MPLAB X IDE by clicking on Tools > Embedded > MPLAB Harmony 3 Configurator.
Select the Harmony framework's path to be loaded.
Click Launch to launch the MHC Configuration tool.
The MHC plugin’s main window for the project will be displayed.

Configure Clock Settings
Launch Clock Easy View by going to the MHC tab in MPLABX IDE and then select Tools > Clock Configuration.

The Clock Easy View window will then appear on your screen.

Enable the 16 MHz Internal Oscillator (OSC16M) and select the 12 MHz ouput in the Oscillator Controller box.

Disable the Digitial Frequecy Locked Loop (DFLL).

Set the OSC16M as the Generic Clock Generator 0 (GCLK0) source clock.

Enable the GCLK1 and set the OSC16M as the GCLK1's clock source.

Enable the GCLK2 and set the OSCULP32K as the GCLK2's clock source. Then, click on the Settings (wheel) button in the top right.

The Advanced Settings window will appear after clicking on the Settings (wheel) button. Check the box for GCLK should keep running in Standby mode.

Select the OSCULP1K as the RTC's source clock.