Migrating ASF SAM C21 Application to MPLAB® Harmony v3 PIC32CM MC: Step 4
Last modified by Microchip on 2023/11/09 09:07
Procedure
When all the previous steps are completed, click the Save button before generating the code.

Save the configuration in its default location when prompted.

Click on the Generate button to generate the code.

Click on the Generate button in the Generate Project window, keeping the default settings as shown below. If prompted to save the configuration, click Save.


As the code is generated, the MPLAB® Harmony Configurator (MHC) displays the progress as shown in the following image.


Build the project. Click on the Clean and Build button
and verify that the project builds successfully.
At this point, you are ready to start implementing your application code.