Getting Started with MPLAB® Harmony v3 Peripheral Libraries on PIC32MK GP MCUs: Step 1
Install the MPLAB® Harmony Configurator (MHC) Plugin in the MPLAB X IDE
Verify that MHC is installed.
Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
- Go to Tools > Embedded.
- You will see MPLAB Harmony 3 Configurator in the menu. If you don't see it in the menu, please install MHC.

Setup MHC Plugin Window Open in Standalone Mode
Go to Tools > Options. You will see the Options window open.


Go to Plugins > Window Manager and select Standalone mode. Click Apply and then click OK.

Create MPLAB Harmony v3 Project Using MPLAB X IDE
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MPLAB Harmony 3 Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.

In the Project Settings window, apply the following settings:
Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLABX .X folder. Enter "pic32mk_gp_db.X" to create a pic32mk_gp_db.X folder.
- Name: enter the project’s logical name as "getting_started_pic32mk_gp_db". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to the configuration settings.


Follow the steps below to set the project’s configuration settings:
Name: Enter the configuration name as "pic32mk_gp_db".
- Target Device: select PIC32MK1024GPE100 as the target device.
- After selecting the target device, click Finish to launch MHC.

While the MHC tool launches, it will ask for the packages to be loaded. In the Load checkboxes list, select the csp package (by default this option is selected) and uncheck all the other packages (if any).
Click Launch to launch the MHC tool with the selected packages.

The MHC plugin’s main window for the project will be displayed in Standalone mode, as shown in the accompanying image.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right-click on the project name getting_started_pic32mk_gp_db and go to Properties.

Make sure that XC32 (v2.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings

A new window, Clock Diagram is opened inside MHC.
Click on the Clock Diagram tab, scroll to the right, and verify that the SYSCLK is set to 120 MHz.