Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Rapid Prototyping with 32-bit MCU-based Curiosity Nano Evaluation Kit Using MPLAB Harmony v3 Software Framework: Step 1
Note: MPLAB Harmony v3 project creation and library code generation are now also supported under Microchip’s famous MPLAB Code Configurator tool. You could also use MPLAB Code Configurator for generating Harmony library code.
Close all existing opened projects before you start creating a new project.
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MPLAB Harmony 3 Project, then click Next.
Figure 5
Information
Note: If 32-bit MPLAB Harmony 3 Project is not displayed, install MHC.
Browse to the folder you downloaded the framework to in the Framework Path edit box. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.
Information
Note: For more information on the content manager, see the "Download MPLAB Harmony Framework" section of the "MPLAB Harmony Configurator Overview" page.
Figure 6
In the Project Settings window, apply the following settings:
Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: <Your_folder>\dev\pic32cmmc_smart_appliance_control.
Folder: Indicates the name of the MPLABX .X folder. Enter "pic32cm_mc00_cnano" to create a pic32cm_mc00_cnano.X folder.
Name: Indicates the name of the project that will be shown in MPLAB X IDE. Enter "smart_appliance_control_pic32cm_mc00_cnano" to set the project's name.
Information
Note: The Path box is read-only. It will update as you make changes to the entries.
Click Next to proceed to Configuration Settings.
Figure 7
Information
Note: Clicking on the Show Visual Help button will open a help window, providing a detailed description of the various fields in the Project Settings window.
Figure 8
5. Follow the steps below to set the project’s Configuration Settings.
Name: Enter the configuration name as "pic32cm_mc00_cnano".
Target Device: Select PIC32CM1216MC00032 as the target device.
Information
Note: You can select the Device Family or enter a partial device name to filter the list in Target Device to make it easier to locate the desired device.
After selecting the target device, click Finish to launch MHC.
Figure 9
Information
Note: The New Project Wizard opens a Configuration Database Setup window to allow you to review the packages that will be used by the current project.
Click Launch to launch the MHC tool with the selected packages.
Figure 10
The MHC plugin’s main window for the project will be displayed.
Figure 11
Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Select project from the Projects tab and File > Project Properties from the main IDE menu.
Figure 12
Make sure that XC32 (v3.00) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.
Figure 13
Information
Note: When configuring the compiler tool chain, make sure to select the latest PIC32CM_MC00_DFP version.
Information
Tool Tip: If you closed MHC accidentally and would like to open it again, go to Tools > Embedded > MPLAB Harmony 3 Configurator in MPLAB X IDE.
Launch Clock Easy View by going to the Tools menu of the MHC window and then selecting Clock Configuration.
Figure 14
A new window, Clock Easy View, is opened inside MHC.
The Clock Easy View window will then appear on your screen. The default CPU clock is set to 48 MHz.
Figure 15
Information
Tool Tip:
The Clock Easy View window can be minimized by clicking the minimize button, as shown in Figure 16.
Figure 16
After minimizing the Clock Easy View window, you can see a small Clock Easy View tab at the bottom-left in MHC, as shown in Figure 17.
Figure 17
The Clock Easy View window can be maximized by clicking the maximize button or by double-clicking on the Clock Easy View window, as shown in Figure 18.
Figure 18
These tips apply to all other plugin managers like Pin Configuration, DMA Configuration, Event System Configuration, and NVIC Configuration.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.