MPLAB® Harmony v3 Peripheral Libraries on SAM E70/S70/V70/V71 MCUs: Getting Started
Objective
MPLAB Harmony v3 is a flexible, fully integrated embedded software development framework for 32-bit microcontrollers (MCUs) and microprocessors (MPUs).
MPLAB Harmony v3 includes the MPLAB Harmony Configurator (MHC) tool, a set of modular, device, and middleware libraries, and numerous example applications, all of which are designed to help you quickly and easily develop powerful and efficient embedded software for Microchip’s 32-bit PIC® and SAM devices.
This tutorial shows you how to use MHC to create an application that gets you started in developing applications on SAM E70/S70/V70/V71 MCUs using the MPLAB Harmony v3 software framework.
The application makes use of SAM E70 Xplained Ultra Evaluation Kit and I/O1 Xplained Pro Extension Kit (sold separately).
The application reads the current room temperature from the temperature sensor on the I/O1 Xplained Pro Extension. The temperature read is displayed on a serial console periodically every 500 milliseconds. The periodicity of the temperature values displayed on the serial console is changed to one second, two seconds, four seconds, and back to 500 milliseconds every time you press the switch SW0 on the SAM E70 Xplained Ultra Evaluation Kit. Also, an LED, LED3, is toggled every time the temperature is displayed on the serial console.
The application you create will utilize:
- Two-Wire Interfaces (TWIHS) (I²C) Peripheral Library to read the temperature from a temperature sensor
- Timer Counter (TC) Peripheral Library to periodically sample temperature sensor data
- Universal Synchronous Asynchronous Receiver Transmitter (USART) and Direct Memory Access (DMA) Peripheral Libraries to print the temperature values on a COM (serial) port terminal application running on a PC
- PORTS Peripheral Library to change the periodicity of temperature sensor data read using SWITCH event and toggle the LED
In the process, the lab will also demonstrate the use of callback functions.
There are two ways to use this tutorial:
- Create the project from scratch:
- Use the provided source files and step-by-step instructions below.
- Use the solution project as an example:
- Build the solution project and download it to the SAM E70 Xplained Ultra Evaluation Kit Board to observe the expected behaviour.
Lab Objectives
- Create an MPLAB Harmony v3 project for a SAM E70 microcontroller from scratch.
- Use MHC to configure and generate MPLAB Harmony v3 Peripheral Libraries code for TC, I²C, USART, DMA, and PORTS peripherals.
- Use the MPLAB Harmony v3 Peripheral Library Application Programming Interfaces (APIs) to implement the application.
Resources
- About SAM E70 Xplained Ultra
- Purchase SAM E70 Xplained Ultra
- About I/O1 Xplained Pro
- Purchase I/O1 Xplained Pro

Hardware Connection Setup
Apart from the hardware tools listed above, the following items are required:
- USB Type-A male to Micro-B male cable for programming/debugging.
Software Tools
Software Tools
For this lab, download the following repositories from GitHub:
Overview
This lab shows you how to create an MPLAB Harmony v3 project from scratch, to configure and generate MPLAB Harmony v3 Peripheral Libraries code for TC, I²C, USART, DMA, and PORTS peripherals. It demonstrates the reading of temperature sensor values from the temperature sensor available on the I/O1 Xplained Pro Extension kit periodically and displays it on a serial console. The periodicity of temperature sampling is changed for every switch press event. Every time the temperature is displayed on the serial console, an LED is toggled.
The application initializes the clock, PORTs, and other peripherals (configured through MHC) by calling the function SYS_Initialize.
The application registers callback event handlers for TWIHS (I²C), DMA, TC, and Parallel Input/Output (PIO) Peripheral Libraries. The callback event handlers are called back by the peripheral libraries when the transaction completion events occur.

The application checks whether the configured TC timer period has expired. On every timer period expiry, the application calls the function TWIHS0_WriteRead to submit a temperature sensor read request to the I²C peripheral library. The I²C peripheral library calls back the registered callback event handler when the latest temperature value is read from the sensor. The application sets a flag in the TC callback event handler.
The application checks the temperature read complete flag to submit a write request to DMA to print the latest temperature value (in a formatted message) onto the serial console over the USART interface.
The application also monitors the pressing of the switch SW0; if a switch press is detected, the application changes the temperature sampling rate from the default 500 milliseconds to one second. On subsequent switch press, the application changes the temperature sampling rate to two seconds, four seconds, and back to 500 milliseconds. The application cycles the temperature sampling rate on every switch press, as shown in Figure 1.2.

The application also toggles user LED LED3 every time the latest temperature value is displayed on the serial console.
Lab Source Files and Solutions
This ZIP file contains the completed solution project for this lab. It also contains the source files needed to perform the lab as per the following step-by-step instructions (see the "Procedure" section on this page).
The contents of this ZIP file need to be placed in the following folder:
<Any directory of your choice>/training/
(example Directory = C:/microchip/harmony/v3.4.0)
Note:
- The project location of an MPLAB Harmony v3 project is independent of the location of the Harmony Framework path (i.e., you need not create or place a Harmony v3 project in a relative path under the Harmony v3 framework folder). The project can be created or placed in any directory of your choice.
- The point above is true because when created, an MPLAB Harmony v3 project generates all the referred source/header files and libraries (if any) under the project folder.
- Both points above contrast with the MPLAB Harmony v2 project location. In MPLAB Harmony v2, the project was supposed to be created in a location under the Harmony framework.
Zip Files
Extracting the ZIP file creates the following folders:
- same70_getting_started contains the lab solution (in the firmware folder) and source files (in the dev_files folder).
- dev_files contains subfolder sam_e70_xult containing application source files and other support files (if any) required to perform the lab (see "Procedure" section).
- firmware contains the completed lab solution project. It can be directly built and downloaded on the hardware to observe expected behavior.
Procedure
Lab Index
Step 1: Create project and configure the SAM E70
- Step 1.1 - Install the MPLAB Harmony Configurator (MHC) Plug-in in MPLAB X IDE
- Step 1.2 - Create MPLAB Harmony v3 Project using MPLAB X IDE
- Step 1.3 - Verify Clock Settings
Step 2: Configure I²C, USART, and TC Peripheral Libraries
- Step 2.1 - Configure TC Peripheral Library
- Step 2.2 - Configure I²C Peripheral Library and I²C pins
- Step 2.3 - Configure USART Peripheral Library and USART pins
- Step 2.4 - Configure DMA Peripheral Library
Step 3: Configure Pins for Switch and LED
- Step 3.1 - Configure switch button pin with PIO to generate an interrupt
- Step 3.2 - Configure LED Pin
- Step 3.3 - Rename the default main file
Step 4: Generate Code
Step 5: Add application code to the project
Step 6: Build, program, and observe the outputs