Harmony v3 Drivers and System Services on SAM E70/S70/V70/V71: Step 3
Configure LED pin
In this step, the user LED on the SAM E70 Xplained Ultra Evaluation Kit will be configured according to the USER_LED design schematic.

Select the MPLAB® Harmony Configurator (MHC) Pin Settings tab, scroll down to PA05 (Pin Number 73) in the Pin ID column, and then configure the PORT pin PA05 as an output pin for LED functionality.

Rename the default main file
Under the Project Graph tab, click on System and give a name of your liking to the default template main file generated by the MHC.

Configure Application Tasks
Go to the Project Graph and select Harmony Core.

The Configuration Options show that for a Harmony Project, MHC automatically enables the generation of application files (app.c and app.h).
Change the Number of Applications to 2.
Expand Application 0 Configuration and rename the default application name to app_sensor.
Expand Application 1 Configuration and rename the default application name to app_eeprom as shown below. Press the Enter key to save the application name.