MPLAB® Harmony v3 Peripheral Libraries on SAM L10: Step 1
Install the MPLAB® Harmony Configurator (MHC) Plug-in in the MPLAB X IDE
Verify that MHC is installed.
• Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB Harmony 3 Configurator in the menu. If you don't see it in the menu, please install MHC.

Create MPLAB Harmony v3 Project using MPLAB X IDE
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MPLAB Harmony 3 Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework to. If you haven't done this, or want to download it to a different folder, click the Launch Framework Downloader button, then click Next.

In the Project Settings window, apply the following settings:
Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLAB X IDE .X folder. Enter sam_l10_xpro to create a sam_l10_xpro.X folder.
- Name: enter the project’s logical name as getting_started_sam_l10_xpro. This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to configuration settings.


Follow the steps below to set the project’s Configuration Settings:
Name: enter the configuration name as sam_l10_xpro.
- Target Device: select ATSAML10E16A as the target device.
- After selecting the target device, click Finish to launch the MHC.

While the MHC tool launches, it will ask for the packages to be loaded. In the Load checkboxes list, select the csp package (by default this option is selected) and uncheck all the other packages (if any).
Click Launch to launch the MHC Configurator tool with the selected packages.

The MHC plugin’s main window for the project will be displayed as shown.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right click on the project name getting_started_sam_l10_xpro and go to Properties.

Make sure that XC32 (v2.20) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to MHC tab in MPLAB X IDE and then select Tools > Clock Configuration.

A new window, Clock Easy View, is opened in the project’s main window.
Click on the Clock Easy View tab, scroll to the right and verify that the Main Clock is set to 32 MHz