Getting Started with USB on SAM MCUs Using MPLAB® Harmony v3: Step 3
Configure Clocks, Pins, and Application Tasks
Configure Clocks
Open the Clock Configuration pane by navigating to MHC > Tools > Clock Configuration.

Figure 1: Open Clock Configuration
Switch MOSCSEL to Main Crystal.

Figure 2: Clock Configuration
Configure Pins
Open the Pin Configuration pane by navigating to MHC > Tools > Pin Configuration.

Figure 3: Open Pin Configuration
Order the pins by Ports for ease of use.

Figure 4: Order by Ports
The LED on the I/O1 Xplained Pro is connected to pin PA0.
Set the function to GPIO.
- Name this pin as "LED".
- Set the direction to Out.
- Set the latch to High.
TWIHS pins, PA3 and PA4, need to be set to the correct function.
- For PA3, set function to TWIHS0_TWD0.
- For PA4, set function to TWIHS0_TWCK0.

Figure 5: LED and TWIHS Pin Config
The LED on the SAM E70 Xplained is connected to pin PC8.

Figure 6: SAM E70 Xplained User LED Schematic
- Set the function to GPIO.
- Name this pin as "USB_LED".
- Set the direction to Out.
- Set the latch to High.

Figure 7: User LED Config
Add and Configure Application Tasks
Go to the Project Graph and click on the Core module.
Under Configuration Options, you will find that MHC automatically generates a default application named app. Set the Number of Applications spinbox to 3 and configure each of them as follows:
Expand Application 0 Configuration and rename the default application name to "app_sensor".
- Expand Application 1 Configuration and rename the default application name to "app_eeprom".
- Expand Application 2 Configuration and rename the default application name to "app_usb".

Figure 8: Configure Application Tasks