Digit Recognition AI/ML Application on SAM E51 IGAT Curiosity Evaluation Kit Using MPLAB® Harmony v3: Step 1

Last modified by Microchip on 2023/11/09 09:08

Contents
Create MPLAB® Harmony v3 Project

In the MPLAB® X IDE, Select File > New Project from the main Integrated Development Environment (IDE) menu.

In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

Select Microchip Embedded

In the Framework Path edit box, browse to the folder where you downloaded the framework. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.

For more information on the content manager, view the video "MPLAB Code Configurator Content Manager for MPLAB Harmony v3 Projects".

Browse to the folder where you downloaded the framework

In the Project Settings window, apply the following settings:

  • Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder
    • The project location can be any valid path, for example: <Folder of your choice>\dev\digit_recognition
  • Folder: Indicates the name of the MPLABX .X folder. Enter sam_e51_igat to create a sam_e51_igat.X folder
  • Name: Enter the project’s logical name as digit_recognition_sam_e51_igat. This is the name that will be shown from within MPLAB X IDE​

Note: The Path box is read-only. It will update as you make changes to the other entries.

Click Next to proceed to Configuration Settings

Set the location, folder, and name settings

Note: Clicking on the Show Visual Help button will open a help window providing a detailed description of the various fields in the Project Settings window.

Click on the show visual help

 

Follow the steps below to set the project’s Configuration Settings.

  • Name: Enter the configuration name as sam_e51_igat
  • Target Device: Select ATSAME51J20A as the target device

​Note: You can select the Device Family or enter a partial device name to filter the list in Target Device to make it easier to locate the desired device.

After selecting the target device, click Finish to create and open the MPLAB Harmony v3 Project

Set the projects configuration settings

In the Project Settings window, apply the following settings:

Before proceeding, set up the compiler toolchain. Click on the Project Properties icon in the digit_recognition_sam_e51_igat - Dashboard tab.

Project dashboard

Make sure that XC32 (v4.00) is selected as the Compiler toolchain for XC32. Click on Apply and then click on OK.

Project properties

After the project is created, click on the MCC button to launch the MCC tool.MCC icon

You will see the Content Manager window, click on the Select MPLAB Harmony button in the Content Manager window to launch Harmony.

MCC content manager wizard

Use the MPLAB® Code Configurator Content Manager for MPLAB Harmony v3 Projects to download the repositories.

For this lab, download the following repositories from GitHub:

  • CSP: The following table shows the summary of contents.
FolderDescription
appsExample applications for CSP library components
archInitialization and starter code templates and data
docsCSP library help documentation
peripheralPeripheral library templates and configuration data
  • DEV_PACKS: The following table shows the summary of contents.
FolderDescription
MicrochipPeripheral register specific definitions
armCore Specific Register Definitions (CMSIS)
  • MHC: The following table shows the summary of contents.
File/FolderDescription
docHelp documentation and licenses for libraries used
np_templatesNew Project templates for supported toolchains
*.jarJava implementations of MHC modules
mhc.jarMain Java executable (run: java -jar mhc.jar -h)
runmhc.batWindows cmd batch file to run standalone MHC Graphical User Interface (GUI)

​Note: The MHC repository is still needed even though you are using the MCC plugin. The MHC repository contains the framework data.

  • CORE: The following table shows the summary of contents.
FolderDescription
appsExample applications for core library components
configCore module configuration scripts
docsCore module library help documentation
driverCore module peripheral device drivers
osalMPLAB Harmony Operating System Abstraction Layer
systemMPLAB Harmony system services
templatesApplication and system file templates
  • GFX: The following table shows the summary of contents.
FolderDescription
LegatoLegato graphics library, drivers, applications, and tools.
BlankBlank graphics interface for third-party graphics libraries
  • TOUCH: MPLAB Harmony 3 Touch Library is a royalty-free software library for developing touch applications on 32-bit microcontrollers with Peripheral Touch Controller peripheral. Developers can use it to integrate the touch-sensing capability into their applications. The library supports both self-capacitance and mutual-capacitance acquisition methods.
  • TFLite Micro Apps: This repository contains the MPLAB® Harmony 3 TensorFlow Lite for Microcontroller (TFLM) Solutions and example applications. The following table shows the summary of contents.
FolderDescription
appsExample applications to demonstrate usage of TFLM with Harmony
configTFLM module configuration files
docsTFLM help documentation
scriptsGoogle Colaboratory notebook for creating Neural Network model
third_partyThird-party component needed for TFLM

If all the required content is available locally, click on the Finish button to launch MCC.

MCC content manager wizard finish

The MCC plugin’s main window for the project will be displayed.

Resource Manager

Resource Manager has two sections one is Project Resources and another one is Device Resources.

Project Resources

The Project Resources pane displays all of the peripherals currently configured for the project. For example, CMSIS and Device Family Packs (DFP). Select the peripheral here, and the peripheral is ready to be configured in the Configuration Options window. In the Project Resources pane, the System module is always present. The System module simplifies the setting of configuration bits and configures the system clock.

Device Resources

The Device Resources pane displays available peripherals for the device. Click on the peripheral you want to add to your project. The peripheral moves to the MCC Project Resources pane and is ready to be configured to your project's requirements. For example, Harmony Peripheral Libraries (PLIBs) for your device.

Versions

Versions shows MPLAB Code Configurator Plugin version information and different libraries along with their version. For example, the supported Harmony v3 library.

Project Graph

Project Graph shows the instantiated components. You can instantiate available components by double-clicking on the component in the Device Resources pane. After successful component instantiation, you can see the instantiated components under the Project Resources pane.

MCC window descriptions

Configuration Options

Configuration Options displays the tree view of the selected component under the Project Graph tab. You can configure the selected component in this section.

Tool Tip: MCC, by default, has the Autosave MCC configuration File option enabled. If you want to disable the MCC autosave option, go to Tools > Options. After opening the Options window, go to Plugins and disable the Autosave MCC configuration file option.

MCC autosave

Back to Top


Verify Clock Settings

From the Project Graph tab, select Plugins > Clock Configuration to launch Clock Easy View.

A new window, Clock Easy View, is opened in the project’s main window.

Tool Tip: Double-click on the Clock Easy View tab to maximize the window.

Open clock configuration window

In Clock Easy View, configure the XOSC0 Oscillator and FDPLL 0 blocks as shown below to generate a 120 MHz CPU clock using an external Oscillator input source.

XOSC0 Oscillator Configuration

XOSC0 Oscillator Configuration

 

For high accuracy and stable clock, the 12 MHz external crystal output is fed to XOSC0 Oscillator.

FDPLL 0 Configuration

FDPLL 0 Configuration

 

Configure the GLCK Generator 1, DFLL, and GLCK Generator 2 blocks as shown below to generate 32 kHz and 48 MHz clocks using an external Oscillator input source. The 32 kHz and 48 MHz clocks will be used in the further steps as TC0 peripheral clock and SERCOM-USART peripheral clock sources respectively.

GLCK Generator 1 Configuration

GLCK Generator 1 Configuration

 

 

DFLL Configuration

DFLL Configuration

 

Also, configure the DFLL advanced settings by clicking on the Settings (gear) button of DFLL.

GLCK Generator 2 Configuration

GLCK Generator 2 Configuration

DFLL advanced settings

Back to Top