Low Power Application on PIC32CM LE00 Using MPLAB® Harmony v3 Peripheral Libraries: Step 4
Configure Power Manager (PM) Peripheral Library
Click on the Resource Management [MCC] tab, In the Device Resources, expand Peripherals > PM.
Double-click, or drag and drop, PM to add the PM peripheral library to the project graph.

Select the PM peripheral library and configure it as shown.
- Set the Performance Level to 0 to reduce the power consumption of the device during Standby mode.
- Enable Force device to run in PL0.
- Enable Put RAM in low power during standby mode.
- Enable Put TrustRAM in low power during standby mode.
- Set the Power Domain Configuration to PDSW Forced ACTIVE
- Enable Dynamic Power Gating: These options allow the device to turn off a power domain during Standby mode if no peripheral contained in this power domain requests its clock.
- Set the Voltage Regulator to operate in Low-power oriented mode during standby to reduce the power consumption of the device even more.

Configure SUPC Peripheral Library
Click on the Resource Management [MCC] tab, In the Device Resources, expand Peripherals > SUPC.
Double-click, or drag and drop, SUPC to add the Supply Controller (SUPC) peripheral library to the project graph.

Select the SUPC peripheral library and configure it as shown.
- Select the VDD Brown-Out Detector (BOD) Configuration
- Select the Select Active mode operation to Sampling Mode. This configuration optimizes and reduces power consumption in Idle mode. And enables monitoring of the power supply to settle at the right voltage on startup to monitor if the voltage goes too low and to react accordingly by triggering a reset, or an interrupt.
- Set the BOD33 Voltage Reference Selection to Selects ULPVREF for the BOD33 for less power consumption which uses Ultra Low power Reference.
- Select the Voltage Regulator (VREG) Configuration
- Set the Voltage Regulator Voltage Reference Selection to Selects ULPVREF for the VREG for less power consumption which uses Ultra Low power Reference.
- Enable the Increase low power mode efficiency bit to optimize and reduce power consumption in Standby mode.

Configure NVMCTRL Peripheral Library
The Non-volatile Memory Controller (NVMCTRL) is added by default to the project graph. Select the NVMCTRL peripheral library and configure it as shown.
- Set Wait States to 1 to read the non-volatile memory. When the device is put in performance level 0, the device clock frequency can not exceed 12 MHz, and one wait-state is required.
- Set the Power Reduction Mode During Sleep to WAKEUP INSTANT. This bit configures the NVMCTRL to wake up the Flash memory when the CPU wakes up from Standby mode, which allows it to reduce device wake-up time.
- Disable the Instruction Cache to reduce the device's wake-up time. When the cache is enabled, the device will look for an instruction to fetch upon interrupt in the cache at first. If the instruction is found, the device wakes up quicker, but if not, a cache miss occurs and the wake up time is longer. This option is good to enable when the instruction to fetch upon an interrupt is always stored in the cache memory, which is not the case here as we have different interrupt sources.

Configure LED
Open the Pin Configuration tab by clicking Project Graph > Plugins > Pin Configuration.

Once the MCC Pin Settings window is opened, scroll down to pin number 59, and then configure this pin as shown:
- Set the pin #59 as GPIO:
- Pin ID = PC19
- Custom Name = LED0
- Function = GPIO
- Direction = Out
- Latch = Low