Low Power Application on PIC32CM LE00 Using MPLAB® Harmony v3 Peripheral Libraries: Step 6
Add Application Code to the Project
The application is already developed and is available in the main_pic32cm_le00.c file under <your unzip folder>/pic32cm_le00_low_power/dev_files/pic32cm_le00_cpro. The main_pic32cm_le00.c file contains the application logic. It also contains placeholders that you will populate with the necessary code in the next step.
- Go to the pic32cm_le00_low_power/dev_files/pic32cm_le00_cpro folder and copy the pre-developed main_pic32cm_le00.c file.
- Replace (over-write) the main.c file of your project available at < Your project folder>/pic32cm-le00_low_power/firmware/src with the copied file.
- Open main.c in MPLAB® X IDE and add the application code by following the steps below:
Implement temperature sensor slave address by adding the following code before the int main (void) function in main.c.
#define TEMP_SENSOR_REG_ADDR 0x00
Under the main.c file, in function main, notice the call to function SYS_Initialize. The generated function SYS_Initialize initializes all the peripheral modules configured through MPLAB® Code Configurator (MCC) and used in the application.

In the main() function, below SYS_Initialize(), add the following code to register callback event handlers, enable the ADC, start the RTC timer, display the message, and enter Standby mode.
SERCOM5_I2C_CallbackRegister (i2cEventHandler, 0);
DMAC_ChannelCallbackRegister (DMAC_CHANNEL_0, dmaChannel0Handler, 0);
ADC_CallbackRegister (adcEventHandler, 0);
ADC_Enable ();
RTC_Timer32Start ();
printf ("\n\n\r---------------------------------------------------------");
printf ("\n\r Low-power Application on PIC32CM LE00 Cpro ");
printf ("\n\r---------------------------------------------------------\n\n\r");
printf ("Enter Standby sleep mode\n\n\r");
PM_StandbyModeEnter ();

Implement the registered callback interrupt handlers for DMA, I²C, ADC, and EIC PLIBs by adding the following code before the int main (void) function in main.c.
{
if(event == DMAC_TRANSFER_EVENT_COMPLETE)
{
isDMATransferComplete = true;
}
}
static void i2cEventHandler (uintptr_t contextHandle)
{
if(SERCOM5_I2C_ErrorGet() == SERCOM_I2C_ERROR_NONE)
{
isTemperatureRead = true;
}
else
{
printf ("There were an error during I2C Transmit. Please ensure that the I/O1 Xplained Pro is connected to the board.\n\n\r");
}
}
static void adcEventHandler (ADC_STATUS status, uintptr_t context)
{
isADCWinMonitorEvent = true;
}
static void EIC_User_Handler (uintptr_t context)
{
sleepMode = true;
}

Inside the while loop, add the code below to unset the isADCWinMonitorEvent flag, turn on the LED0, print the message, and submit an I²C transfer to read the temperature sensor value. When the submitted request is completed, the i2cEventHandler callback function declared in step 2 is called.
{
isADCWinMonitorEvent = false;
LED0_Clear ();
printf ("ADC_WINMON Interrupt Detected. Wake-up from sleep mode.\n\r");
SERCOM5_I2C_WriteRead (TEMP_SENSOR_SLAVE_ADDR, &i2cWrData, 1, i2cRdData, 2);
LED0_Set ();
PM_StandbyModeEnter ();
}

Inside the while loop, add the code below to unset the isTemperatureRead flag, store the temperature read into the temperatureVal variable, fill uartTxBuffer with the converted temperature value in degrees Fahrenheit, and transmit this value to the terminal through the SERCOM3 USART peripheral by using the DMA.
{
isTemperatureRead = false;
temperatureVal = getTemperature (i2cRdData);
sprintf ((char*)uartTxBuffer, "Temperature = %02d F \r\n", temperatureVal);
while (!SERCOM3_USART_TransmitterIsReady());
DMAC_ChannelTransfer (DMAC_CHANNEL_0, uartTxBuffer, (const void*)&(SERCOM3_REGS->USART_INT.SERCOM_DATA), sizeof(uartTxBuffer));
}

Inside the while loop, add the code below to unset the isDMATransferComplete flag, print the message, turn off the LED0, and put the device in Standby mode by using the PM_StandbyModeEnter () function.
{
isDMATransferComplete = false;
printf("DMA transfer completed. Entering in Standby sleep mode.\n\n\r");
LED0_Set ();
PM_StandbyModeEnter ();
}

Inside the while loop, add the code below to unset the sleepMode flag, toggle pin PC28, print the message, turn off the LED0, and put the device in Idle mode by using the PM_IdleModeEnter () function.
{
sleepMode = false;
printf ("SW1 button pressed. Entering Idle sleep mode.\n\n\r");
LED0_Set ();
PM_IdleModeEnter ();
}

You are now ready to build the code and observe the results!