Low Power Application on SAM E54 Using MPLAB® Harmony v3 Peripheral Libraries: Step 2
Configure Real-Time Clock (RTC) Peripheral Library
Click on the Resource Management [MCC] tab, In the Device Resources, expand Harmony > Peripherals > RTC.
Double click or drag and drop RTC to add the RTC Peripheral Library (PLIB) to the project graph.

In Clock Easy View, verify the RTC clock is set to run at 1 kHz internal ultra-low-power clock.
When a module is added to the project graph, MPLAB® Code Configurator (MCC) automatically enables the clock to the module. The default RTC clock source is an internal 1 kHz ultra-low-power clock (OSCULP1K).

Go back to the project graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.

Configure I²C Peripheral Library, I²C Pins, and Verify I²C Clock
Click on the Resource Management [MCC] tab, In the Device Resources, expand Harmony > Peripherals > SERCOM.
Double click on SERCOM3 to add the SERCOM instance 3 to the project.

Select the SERCOM 3 Peripheral Library and configure it for the I²C protocol.

Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Select the MCC Pin Settings tab and sort the entries by Ports names.

Now, select the MCC Pin Table tab and then scroll down to the SERCOM3 module as follows:
Enable I²C Clock (TWI_SCL)(SERCOM3_PAD1) on PA23 (Pin #93)
Enable I²C Data (TWI_SDA)(SERCOM3_PAD0) on PA22 (Pin #92)

In Clock Easy View, open the Peripheral Clock Configuration by clicking on the button Peripheral Clock Configuration.

Once the window is opened, scroll down to the SERCOM3_CORE peripheral and select GCLK2 (1 MHz) as the source clock to generate the peripheral clock frequency.

Configure Universal Synchronous Asynchronous Receiver Transmitter (USART) Peripheral Library, USART Pins, and Verify USART Clock
Click on the Resource Management [MCC] tab, In the Device Resources, expand Harmony > Peripherals > SERCOM.
Double click on SERCOM2 to add the SERCOM instance 2 to the project.

Associate STDIO tool with SERCOM instance 2 (USART) peripheral by right clicking on the yellow diamond.


Select the SERCOM2 Peripheral Library in the Project Graph window and verify default SERCOM Operation Mode configuration is set as USART and configure it.

Verify the default baud rate is set to 115200 Hz.
Select the Pin Table tab and then scroll down to the SERCOM2 module as follows:
Enable USART_TX (SERCOM2_PAD0) on PB25 (Pin #101)
Enable USART_RX (SERCOM2_PAD1) on PB24 (Pin #100)

In Clock Easy View, open the Peripheral Clock Configuration by clicking on the button Peripheral Clock Configuration.

Once the window is opened, scroll down to the SERCOM2_CORE peripheral and select GCLK2 (1 MHz) as the source clock to generate the peripheral clock frequency.

Configure DMA Peripheral Library
Open the DMA Configuration tabs by clicking Project Graph > Plugins > DMA Configuration.

Click on the DMA Settings tab. Configure DMA Channel 0 to transfer the application buffer to the USART TX register. The DMA transfers one byte from the user buffer to the USART transmit buffer on each trigger.
Based on the trigger source, the DMA channel configuration is automatically set by MCC.
- Enable Interrupts: In this Tab, SERCOM2 (as USART) Interrupt is enabled.
Trigger Action: action taken by DMA on receiving a trigger.
- One beat transfer: generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- One block transfer: generally used during the memory-to-memory transfer on a software trigger.
Source Address Mode, Destination Address Mode: select whether to increment Source/Destination Address after every transfer. Automatically set by the MCC, based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented, and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed, and the Destination Address is incremented.
Beat Size: size of one beat. The default value is 8-bits. For example:
- If the SPI peripheral is configured for 16-bit/32-bit mode, then the beat size must be set to 16-bits/32-bits respectively.
Burst Length: this is a very fast data transfer mode. It can perform up to 16 transfers (beats) before releasing the control of the system bus back to the CPU. The default value of burst length is a single beat (one transfer).
- In the default configuration, USART is configured for one-byte data at a time. So, the burst length is configured as a single beat.
FIFO Threshold: FIFO threshold level determines the size when the data in the internal DMA FIFO should be transferred to/from memory.
- When the size of the data filled (in the internal DMA FIFO) becomes equal to the FIFO threshold size, the actual burst transfer (from the internal DMA buffer to USART peripheral) takes place, thereby improving the overall performance.
- In the default configuration, the DMA transfers 1 beat of data as burst transfer.
Click on Add Channel to add the DMA channel and configure the DMA channel.