Low Power Application on SAM E54 Using MPLAB® Harmony v3 Peripheral Libraries: Step 7
Build and Program the Application
Clean and build your application by clicking on the Clean and Build button as shown.
![]()
Program your application to the device by clicking on the Make and Program button as shown.




In the Serial Port window, verify that the Baud Rate is set to 115200 and other elements are set as shown in the image, then press OK.

Now that the serial console is configured, reset the board, and verify the application title message is displayed.

Cover the light sensor on the I/O Xplained Pro board by placing your hand over it (or another element to put the light sensor in a dark environment) to print the temperature and message on the terminal. You should see the following messages (containing the temperature value in °F) on the terminal every 500 milliseconds for the duration the light sensor is covered:

Observe Current Consumption on Data Visualizer
Open the Data Visualizer application from your PC and select the connected SAM E54 Xplained Pro board on the DGI Control Panel, then click on Connect. The Data Visualizer will then start searching for protocols from the SAM E54 Xplained Pro board through the EDBG.

Once the Data Visualizer is connected to the SAM E54 EDBG, different interfaces will appear. Select the Power interface and click on the Start button to start measuring the power consumption of the device.

Ensure that the jumpers for Current Measurement on the SAM E54 Xplained Pro are set to MEASURE for the MCU and BYPASS for the I/Os.

The Power Analysis window will appear on the Data Visualizer tool interface.

The accompanying image shows the device in Standby mode with its measured power consumption. You can observe small peaks that illustrate the 500 milliseconds Real-Time Clock (RTC) timer expiry.

Cover the light sensor on the I/O Xplained Pro board by placing your hand over it (or another element) to print the temperature on the terminal and observe the power consumption of the device.

Press the SW0 button to switch from Standby mode to Idle mode. The following image shows the transition of the power consumption from Standby mode to Idle mode.

The following image shows the device in Idle mode with a measured power consumption of 1599.4 µA.

Place your hand over the light sensor. The device will wake up on the next ADC window monitor interrupt, read and print data on serial, and then re-enter Standby mode. The following image shows the transition of the power consumption by switching from Idle mode to Standby mode.

Results
You successfully created a low power application using the SAM E54 Xplained Pro Evaluation Kit and I/O1 Xplained Pro Kit and experienced how, where, and which Low Power mode to use depending on the application requirements such as power and wake up response times.
Analysis
In this lab, you have successfully created a project from scratch, added Peripheral Libraries (PLIBs), and learned how to use an Event System to drive events received from the peripherals without CPU intervention. You also learned how to configure a device to work in Sleep modes and measure wake-up time.
Conclusions
In this tutorial, you discovered how to configure the device to work in Sleep modes, this tutorial can be used as a reference when you develop a real-time application where the power and wake up response time plays a crucial role.