Low Power Application on SAMC2x Using MPLAB® Harmony v3 Peripheral Libraries: Step 1
Verify whether MPLAB® Code Configurator (MCC) Plugin is installed in MPLAB® X IDE
Verify that MCC is installed
• Launch MPLAB® X IDE from the Microsoft Windows® Start menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB® Code Configurator v5: Open/Close in the menu.
If you don't see it in the menu, install MCC.
Create MPLAB Harmony v3 Project using MPLAB® X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.
In the Framework Path edit box, browse to the folder where the framework has been downloaded, then click Next.

In the Project Settings window, apply the following settings:
- Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev\samc21_low_power.
- Folder: Indicates the name of the MPLABX .X folder. Enter "sam_c21_xpro" to create a sam_c21_xpro.X folder.
- Name: Enter the project’s logical name as "low_power_sam_c21_xpro". This is the name that will be shown from within MPLAB X IDE.
- Click Next to proceed to Configuration Settings.
Follow the steps below to set the project’s Configuration Settings.
- Name: Enter the configuration name as “sam_c21_xpro”.
- Target Device: Select ATSAMC21J18A as the target device.
- After selecting the target device, click Finish to launch MCC.
The MCC content manager window is displayed. In this click Select MPLAB Harmony (by default this option is selected).
Click Finish to launch the MCC Configurator tool with the packages.
The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right click on the project name low_power_sam_c21_xpro.
Go to Set Configuration and click on Customize.
Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32 and select the Simulator.
Click on Apply and then click on OK.
Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in MPLABX IDE and then select Plugins > Clock Configuration.
A new window, Clock Easy View, is opened in the project’s main window.
Click on the Clock Easy View tab, scroll to the right, and verify that the Main Clock is set to 48 MHz.