Low Power Application on SAM L21 Using MPLAB® Harmony v3 Peripheral Libraries: Step 1
Create a Project and Configure the SAM L21
Verify that MPLAB® Code Configurator (MCC) is installed in MPLAB X IDE
• Launch MPLAB X IDE from the Microsoft® Windows® Start menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB Code Configurator v5 in the menu.

Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework, then click Next.
In the Project Settings window, apply the following settings:
- Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, <Your_folder>\dev\saml21_low_power.
- Folder: Indicates the name of the MPLABX .X folder. Enter "sam_l21_xpro" to create a sam_l21_xpro.X folder.
- Name: Indicates the name of the project that will be shown in the MPLAB X IDE. Enter "low_power_sam_l21_xpro" to set the project's name.
- Click Next to proceed to Configuration Settings.


Follow the steps below to set the project’s Configuration Settings.
- Name: Enter the configuration name as "sam_l21_xpro".
- Target Device: Select ATSAML21J18B as the target device.
- After selecting the target device, click Finish to launch MCC.

While the MCC tool launches, Click on Select MPLAB Harmony content type.

Click on the Finish Button in the MCC Content Manager Wizard.
The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right-click on the project name low_power_sam_l21_xpro and go to Properties.

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Configure Clock Settings
Launch Clock Easy View by going to Project Graph in MPLABX IDE and then select Plugins > Clock Configuration.

The Clock Easy View window will then appear on your screen.

Enable the 16 MHz Internal Oscillator (OSC16M) and select the 12 MHz output in the Oscillator Controller box.

Disable the Digital Frequency Locked Loop (DFLL).

Set the OSC16M as the Generic Clock Generator 0 (GCLK0) source clock.

Enable the GCLK1 and set the OSC16M as the GCLK1's clock source.

Enable the GCLK2 and set the OSCULP32K as the GCLK2's clock source. Then, click on the Settings (wheel) button in the top right.

The Advanced Settings window will appear after clicking on the Settings (wheel) button. Check the box for GCLK should keep running in Standby mode.

Select the OSCULP1K as the RTC's source clock.