Low Power Application on SAM L21 Using MPLAB® Harmony v3 Peripheral Libraries: Step 2
Configure RTC, I2C, USART, and DMA Peripheral Libraries
Configure RTC Peripheral Library
Click on the Resource Management [MCC] tab, In the Device Resources, expand Peripherals > RTC.
Double-click or drag and drop RTC to add the RTC peripheral library (PLIB) to the project graph.

Verify that the RTC clock is set to run at 1 kHz using the 1 kHz Ultra Low Power Internal Oscillator (OSCULP1K).

Go back to the project graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.

Configure I²C Peripheral Library, I²C Pins, and Verify I²C Clock
Configure I²C Peripheral
Click on the Resource Management [MCC] tab, In the Device Resources, expand Peripherals > SERCOM.
Double-click on SERCOM2 or drag and drop to add SERCOM instance 2 to the project.

Select the SERCOM 2 peripheral library and configure it for the I²C protocol:

Configure I²C Pins
Click Project Graph > Plugins > Pin Configuration to open the Pin Configuration tabs.

Once the MCC Pin Settings window is opened, find the Order drop-down list, and select Pins to sort the entries by port names.

Now, select the MCC Pin Table tab and then scroll down to the SERCOM2 module as shown:
- Enable I²C data (I2C_SDA) on PA08 (pin #17)
- Enable I²C clock (I2C_SCL) on PA09 (pin #18)

Go back to the Pin Settings table and customize the PA08 and PA09 pins names as listed:
- Pin ID: PA08
- Custom Name: I2C_SDA
- Pin ID: PA09
- Custom Name: I2C_SCL

Verify I²C Clock
Open the Clock Configuration tab by clicking Project Graph > Plugins > Clock Configuration.

Open the Peripheral Clock Configuration tab by clicking on the button in the Peripheral Clock Selection.
Once the window is opened, scroll down to the SERCOM2_CORE peripheral and select GCLK0 (12 MHz) as the source clock to generate the peripheral clock frequency.
Configure the USART Peripheral Library, and USART Pins, and Verify the USART Clock
Configure USART Peripheral
Under the left tab Resource Management (MCC), go to Device Resources and expand Libraries > Harmony > Peripherals > SERCOM.
Double-click on SERCOM3 or drag and drop to add SERCOM instance 3 to the project.

Under the Resource Management (MCC) tab, go to Device Resources and expand Libraries > Harmony > Tools and double-click on STDIO or drag and drop to add the STDIO tool to the project.

Connect the SERCOM3 USART output to the STDIO USART input.
Select the SERCOM 3 peripheral library in the Project Graph and configure it for the USART protocol.
Configure USART Pins
Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Now, select the MCC Pin Table tab and then scroll down to the SERCOM3 module as listed below:
- Enable USART Transmit (SERCOM3_TX) on PA22 (pin #43)
- Enable USART Receive (SERCOM3_RX) on PA23 (pin #44)

Go back to the Pin Settings table and customize the PA22 and PA23 pins names as indicated below:
- Pin ID: PA22
- Custom Name: SERCOM3_TX
- Pin ID: PA23
- Custom Name; SERCOM3_RX

Verify USART Clock
Open the Clock Configuration tab by clicking Project Graph > Plugins > Clock Configuration.

Open the Peripheral Clock Configuration tab by clicking on the button in the Peripheral Clock Selection.

Once the window is opened, scroll down to the SERCOM3_CORE peripheral and select GCLK0 (12 MHz) as the source clock to generate the peripheral clock frequency.

Configure DMA Peripheral Library
Open the DMA Configuration tabs by clicking Project Graph > Plugins > DMA Configuration.

Click on the DMA Settings tab. Configure DMA Channel 0 to transfer the application buffer to the USART TX register. The DMA transfers one byte from the user buffer to the USART transmit buffer on each trigger.
Based on the trigger source, the DMA channel configuration is automatically set by MCC.
- Trigger Action: Action taken by DMA on receiving a trigger.
- One beat transfer: Generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- One block transfer: Generally used during the memory-to-memory transfer on a software trigger.
- Source Address Mode, Destination Address Mode: Select whether to increment the Source/Destination Address after every transfer. Automatically set by MCC based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented, and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed, and the Destination Address is incremented.
- Beat Size: Size of one beat. The default value is 8 bits. For example:
- If the SPI peripheral is configured for 16-bit/32-bit mode, then the beat size must be set to 16/32 bits respectively.
- Enable Interrupts: In this Tab, SERCOM3 (as USART) Interrupt is enabled.