Arm® TrustZone® Technology Getting Started Application on PIC32CK SG01: Step 2
Configure Secure Real-Time Clock (RTC) Peripheral Library
Under the bottom left Device Resources tab, expand Harmony > Peripherals > RTC.
Double-click or drag and drop RTC to add the RTC Peripheral Library (PLIB) to the Project Graph.

Figure 1
In the Clock Easy view, verify the RTC clock is set to run at 1 kHz internal ultra-low-power clock.
When a module is added to the Project Graph, MPLAB® Code Configurator (MCC) automatically enables the clock to the module. The default RTC clock source is an internal 1 kHz ultra-low-power clock (OSCULP1K).

Figure 2
Go back to the Project Graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.

Figure 3
Configure Secure I²C Peripheral Library and Secure I²C pins
Under the Device Resources tab, expand Harmony > Peripherals > SERCOM.
Double-click on SERCOM4 to add the SERCOM instance 4 to the project.

Figure 4
Select the SERCOM 4 Peripheral Library and configure it for the I²C protocol as shown in Figure 5.

Figure 5
Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Figure 6
Select the Pin Settings tab and sort the entries by Ports, as shown in Figure 7.

Figure 7
Now, select the Pin Settings tab and then scroll down to the SERCOM4 module as follows:
- Enable I²C Data (I²C_SDA) (SERCOM_PAD0) on PB09 (Pin #71) as Secure mode.
- Enable I²C Clock (I²C_SCL) (SERCOM_PAD1) on PB10 (Pin #72) as Secure mode.

Figure 8
This completes the configuration of the I²C peripheral library. The application code will use the I²C PLIB Application Programming Interfaces (APIs) to read temperature from the temperature sensor.
Configure Non-Secure Universal Synchronous Asynchronous Receiver Transmitter (USART) Peripheral Library and USART pins
Under the tab Device Resources tab, expand Harmony > Peripheral > SERCOM.
Double-click on SERCOM5 to add the SERCOM instance 5 to the project.

Figure 9
Select the SERCOM5 Peripheral Library in the Project Graph and verify default SERCOM Operation Mode configuration is set as USART. Configure it as shown in Figure 10.

Figure 10
Verify the default baud rate is set to 115200 Hz.
Select the Pin Settings tab and then scroll down to the SERCOM5 module.
- Enable USART_TX (SERCOM_PAD0) on PA24 (Pin #17) as NonSecure Mode.
- Enable USART_RX (SERCOM_PAD1) on PA25 (Pin #20) as NonSecure Mode.

Figure 11
Configure Non-Secure DMA Peripheral Library
Configure DMA by selecting the System block in the Project Graph. In Configuration Options navigate to DMA.

Figure 12
Expand DMA
Enable DMA Channel 0.
- Enable DMA Channel 1.

Figure 13
- Expand DMA Channel 0 and configure it to transmit the application buffer to the USART TX register. The DMA transfers one byte from the user buffer to the USART transmit buffer on each trigger.
- Expand DMA Channel 1 and configure it to receive the USART RX register data to the application receive buffer. The DMA transfers one byte from the USART receive buffer to the user buffer on each trigger.

Figure 14
Based on the trigger source, the DMA channel configuration is automatically set by MCC.
- Trigger Action: Action taken by DMA on receiving a trigger.
- Cell Transfer: The number of bytes transferred when a DMA channel has a transfer initiated before waiting for another event. A cell transfer is comprised of one or more transactions. Generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- Block transfer: The number of bytes transferred when a channel is enabled. The number of bytes is the larger of either Source or Destination size. A block transfer is comprised of one or more cell transfers. Generally used during the memory-to-memory transfer on a software trigger.
- Source Address Mode, Destination Address Mode: Select whether to increment the Source/Destination Address after every transfer. Automatically set by MCC based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented, and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed, and the Destination Address is incremented.
Launch NVIC Configuration by selecting Project Graph > Plugins > NVIC Configuration.

Figure 15
Click on the NVIC Settings tab. Verify that the DMA0_PRI1 (DMA Channel 0) and DMA0_PRI2 (DMA Channel 1) as NON-SECURE projects.

Figure 16