Arm® TrustZone® Technology Getting Started Application on PIC32CM LS60: Step 6
Add Application Code to the Non-Secure Project
The application is already partially developed and is available in the main.c file under <your unzip folder>/pic32cm_ls60_cpro_tz_getting_started/dev_files/Non-secure. The main.c file contains the application logic. It also contains placeholders that you will populate with the necessary code in the next step.
Go to the pic32cm_ls60_cpro_tz_getting_started/dev_files/Non-secure folder and copy the pre-developed main.c file.
Replace the main.c file of your project available at <Your project folder>/pic32cm_ls60_cpro_tz_getting_started/firmware/src by overwriting it with the copied file.
Go to the pic32cm_ls60_cpro_tz_getting_started/dev_files/Non-secure/trustZone folder and copy the pre-developed nonsecure_entry.h file.
Replace the nonsecure_entry.h file of your project available at <Your project folder>/pic32cm_ls60_cpro_tz_getting_started/firmware/src/trustZone by over-writing it with the copied file.
Open the tz_pic32cm_ls60_cpro project main.c in MPLAB® X IDE and add the application code by following the steps:
Under the main.c file, in function main, notice the call to the SYS_Initialize function.
The generated SYS_Initialize function initializes all the peripheral modules used in the non-secure application, which is configured through MPLAB Code Configurator (MCC).

Figure 1
In the main() function, below SYS_Initialize(), add the following code to register callback event handlers.
DMAC_ChannelCallbackRegister(DMAC_CHANNEL_1, usartRxDmaChannelHandler, 0);
Following the addition of the code above, add the function call to receive a character from the serial terminal.
uartRxBuffer, 1);

Figure 2
Implement the registered callback event handlers for the DMA PLIB (for both channels) by adding the following code before the non-secure main() function in main.c.
{
if (event == DMAC_TRANSFER_EVENT_COMPLETE)
{
isUSARTTxComplete = true;
}
}
static void usartRxDmaChannelHandler(DMAC_TRANSFER_EVENT event, uintptr_t contextHandle)
{
if (event == DMAC_TRANSFER_EVENT_COMPLETE)
{
isEEPROMReadReq = true;
}
}

Figure 3
Implement the Electrically Erasable Programmable Read-Only Memory (EEPROM) data print function to print the last five temperature values received from the secure application.
{
char* pBuffer = (char*)nonSecureUartTxBuffer;
uint8_t len;
uint8_t i;
len = sprintf((char*)pBuffer, "EEPROM:");
for (i = wrIndex; i < EEPROM_MAX_LOG_VALUES; i++)
{
len += sprintf((char*)&pBuffer[len], "%dF|", (int8_t)pTemperatureValue[i]);
}
if (wrIndex > 0)
{
for (i = 0; i < wrIndex; i++ )
{
len += sprintf((char*)&pBuffer[len], "%dF|", (int8_t)pTemperatureValue[i]);
}
}
len += sprintf((char*)&pBuffer[len], "\r\n");
DMAC_ChannelTransfer(DMAC_CHANNEL_0, nonSecureUartTxBuffer, \
(const void *)&(SERCOM3_REGS->USART_INT.SERCOM_DATA), \
strlen((const char*)nonSecureUartTxBuffer));
}

Figure 4
Add the following code in the while() super-loop to print the received temperature values from the secure application on the serial terminal.
{
/* Maintain state machines of all polled MPLAB Harmony modules. */
DMAC_ChannelTransfer(DMAC_CHANNEL_0, nonSecureUartTxBuffer, \
(const void *)&(SERCOM3_REGS->USART_INT.SERCOM_DATA), \
strlen((const char*)nonSecureUartTxBuffer));
}

Figure 5
Add the following code to request the secure application to read the last five values stored in the EEPROM by using Non-Secure Callables (NSCs) when a character on the serial terminal is received.
{
isEEPROMReadReq = false;
readEEPROMTemperatureDataReq(&eepromRxBuffer[0]);
}

Figure 6
Add the following code to print the last five temperature values on the serial terminal and also a function call to receive a character from the serial terminal through keyboard press. Then the requested last five stored temperature values are read from the EEPROM in the secure application. Along with the printing function, an LED1 is toggled after every keyboard press action.
{
isEEPROMReadReq = false;
eepromPrintTemperature(&eepromRxBuffer[0], wrIndex);
DMAC_ChannelTransfer(DMAC_CHANNEL_1, (const void *)&(SERCOM3_REGS->USART_INT.SERCOM_DATA), \
&uartRxBuffer[0], 1);
LED1_Toggle();
}
secureAppEntry();

Figure 7
Under Header Files > trustZone, in the nonsecure_entry.h file, add the following code to extern the NSCs to access and request the secure application from the non-secure application.
extern bool readTemperatureData(uint8_t *lcluartTxBuffer);
extern void readEEPROMTemperatureDataReq(uint8_t *temperatureBuf);
extern bool getEEPROMTemperatureDataReadStatus(uint8_t *LclWrIndex);
extern void secureAppEntry(void);

Figure 8
You are now ready to build the code!