Getting Started with MPLAB® Harmony v3 Peripheral Libraries on PIC32MK GP MCUs: Step 1
Create MPLAB® Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.

In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

Browse to the folder you downloaded the framework to in the Framework Path edit box. Then click Next.
- The path to your Harmony 3 installation folder should already be populated. if not, create a folder somewhere on your computer, like C:\harmony3, and point the project to that path.
- The Harmony 3 necessary files will be downloaded to that path later during these steps

In the Project Settings window, apply the following settings:
- Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev\pic32mk_getting_started.
- Folder: indicates the name of the MPLABX .X folder. Enter "pic32mk_gp_db" to create a pic32mk_gp_db.X folder.
- Name: enter the project’s logical name as "getting_started_pic32mk_gp_db". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to the configuration settings.


Follow the steps below to set the project’s configuration settings:
- Name: enter the configuration name as "pic32mk_gp_db".
- Target Device: select PIC32MK1024GPE100 as the target device.
- After selecting the target device, click Finish to launch MCC.

The MCC content manager window is displayed. In this click Select MPLAB Harmony (by default this option is selected).

Click Finish to launch the MCC tool with the packages.

The MCC plugin’s main window for the project will be displayed in Standalone mode, as shown in the image.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right click on the project name "getting_started_pic32mk_gp_db".
Go to Set Configuration and Click on the Customize..

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in the MPLAB X IDE and then select Plugins > Clock Configuration.

A new window, Clock Diagram is opened inside MCC.
Click on the Clock Diagram tab, scroll to the right and verify that the SYSCLK is set to 120 MHz.