MPLAB® Harmony v3 Peripheral Libraries on PIC32MX 470: Step 1
Install the MPLAB® Code Configurator (MCC) Plug-in in MPLAB X IDE
Verify that MCC is installed.
Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
Go to Tools > Embedded.
You will see MPLAB Code Configurator v5 in the menu. If you don't see it in the menu, please install MCC.

Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework to. If you haven't done this, or want to download it to a different folder, click the Launch Content Manager button, then click Next.

In the Project Settings window, apply the following settings:
- Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLABX .X folder. Enter "pic32mx470_curiosity" to create a pic32mx470_curiosity.X folder.
- Name: enter the project’s logical name as "getting_started_pic32mx470_curiosity". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to configuration settings.


Follow the steps below to set the project’s configuration settings:
- Name: enter the configuration name as "pic32mx470_curiosity".
- Target Device: select PIC32MX470F512H as the target device.
- After selecting the target device, click Finish to launch MCC.

While the MCC tool launches, Click on Select MPLAB Harmony content type.

Click on the Finish Button in the MCC Content Manager Wizard.

The MCC plug-in’s main window for the project will be displayed in Standalone mode, as shown in the following image.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right-click on the project name getting_started_pic32mx470_curiosity and go to Set Configuration> Customize.

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to Project Graph in MPLABX IDE and then select Plugins > Clock Configuration.

A new window, Clock Diagram is opened inside MCC.
Click on the Clock Diagram tab, scroll to the right, and verify that the SYSCLK is set to 96 MHz.