MPLAB® Harmony v3 Peripheral Libraries on PIC32MZ EF: Step 1
Create Project and Configure the PIC32MZ EF
Install the MPLAB® Code Configurator (MCC) Plugin in MPLAB X IDE or verify that MCC is installed.
- Launch MPLAB X IDE from the Windows® Start menu. Close any projects and files that are currently open.
- Go to Tools > Embedded.
- You will see MPLAB Code Configurator v5: Open/Close in the menu.

If you don't see it in the menu, install MCC.
Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder where the framework has been downloaded, then click Next

In the Project Settings window, apply the following settings:
- Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, e.g., C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLAB X .X folder. Enter "pic32mz_ef_curiosity_v2" to create a pic32mz_ef_curiosity_v2.X folder.
- Name: enter the project’s logical name as "getting_started_pic32mz_ef_curiosity_v2". This is the name that will be shown within the MPLAB X IDE.
- Click Next to proceed to configuration settings.


Follow the steps below to set the project’s Configuration Settings:
- Name: enter the configuration name as "pic32mz_ef_curiosity_v2".
- Target Device: select PIC32MZ2048EFM144 as the target device.
- After selecting the target device, click Finish to launch the MCC.

The MCC content manager window is displayed. In this, click Select MPLAB Harmony (by default this option is selected).

Click Finish to launch the MCC tool with the packages.

The MCC plugin’s main window for the project will be displayed as shown in the accompanying image.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right click on the project name getting_started_pic32mz_ef_curiosity_v2.
Go to Set Configuration and click on the Customize option.

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32 and select the Simulator.
Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in MPLABX IDE and then select Plugins > Clock Configuration..

A new window, Clock Easy View, is opened in the project’s main window.
Click on the Clock Easy View tab, scroll to the right, and verify that the SYSCLK is set to 200 MHz