MPLAB® Harmony v3 Peripheral Libraries on SAMC2x: Step 2
Configure I2C, USART, and RTC Peripheral Libraries
Configure RTC Peripheral Library
Click on the Resource Management [MCC] tab, In the Device Resources, expand Peripherals > RTC.
Double-click or drag and drop RTC to add the RTC peripheral library (PLIB) to the project graph.
Verify that the RTC clock is set to run at 1 kHz internal ultra-low power clock.
When a module is added to the project graph, MPLAB® Code Configurator (MCC) automatically enables the clock to the module. The default RTC clock source is internal 1 kHz ultra-low power clock (OSCULP1K).
Go back to the project graph and configure the RTC PLIB to generate a compare interrupt every 500 milliseconds.
Configure I²C Peripheral Library and I²C pins
Under the left tab Resource Management (MCC), go to Device Resources and expand Libraries > Harmony > Peripherals > SERCOM.
Double-click on SERCOM5 to add the SERCOM instance 5 to the project.

Select the SERCOM5 peripheral library and configure it for I²C protocol as shown.
Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Select the Project Graph > Plugins > Pin Settings tab and sort the entries by Port names as shown:

Now, select the Plugins > Pin Table tab and then scroll down to the SERCOM5 module as shown:
- Enable I²C Clock (TWI_SCL) on PB17 (Pin #65)
- Enable I²C Data (TWI_SDA) on PB16 (Pin #64)

Configure USART Peripheral Library and USART pins
Under the left tab Resource Management (MCC), go to Device Resources and expand Libraries > Harmony > Peripherals > SERCOM.
Double-click on SERCOM4 to add the SERCOM instance 4 to the project.

Select the SERCOM4 peripheral library in the Project Graph and configure it for Universal Synchronous Asynchronous Receiver Transmitter (USART) protocol as shown:

Verify the default baud rate is set to 115200 Hz.
Select the Pin Table tab and then scroll down to the SERCOM4 module as shown:
Enable USART_TX on PB10 (Pin #30).

Configure DMA Peripheral Library
From the Project Graph tab, select Plugins > DMA Configuration to launch the DMA Configuration window.

Click on the DMA Settings tab. Configure DMA Channel 0 to transfer application buffer to the USART TX register. The DMA transfers one byte from user buffer to USART transmit buffer on each trigger.
Based on the trigger source, the DMA channel configuration is automatically set by MCC.
- Trigger Action: Action taken by DMA on receiving a trigger.
- One beat transfer: Generally used during a memory-to-peripheral or peripheral-to-memory transfer.
- One block transfer: Generally used during the memory-to-memory transfer on a software trigger.
- Source Address Mode, Destination Address Mode: Select whether to increment Source/Destination Address after every transfer. Automatically set by MCC based on the trigger type. For example:
- If the trigger source is USART transmit, then the Source Address is incremented and the Destination Address is fixed.
- If the trigger source is USART receive, then the Source Address is fixed and the Destination Address is incremented.
- Beat Size: Size of one beat. The default value is 8-bits. For example:
- If the Serial Peripheral Interface (SPI) peripheral is configured for 16-bit/32-bit mode, then the beat size must be set to 16-bits/32-bits respectively.
- Enable Interrupts: In this Tab, SERCOM4 (as USART) Interrupt is enabled.