MPLAB® Harmony v3 Peripheral Libraries on SAMC2x: Step 3
Configure Pins for Switch and LED
Configure the switch button pin with EIC
In the Plugins, select the Pin Settings tab and then scroll down to 67 in the Pin Number column and configure the PORT pin PB19 as an external interrupt pin for switch functionality as shown in the accompanying image. The internal pull-up is enabled to avoid false edge detection as there is no external pull-up on the SAMC21N Xplained Pro Evaluation Kit.

Select the Project Graph tab.
Add the External Interrupt Controller (EIC) to the project.
Under the left side tab, Resource Management (MCC), go to Device Resources and expand Libraries > Harmony > Peripherals > EIC.
Select and double-click on EIC to add the EIC module to the project.

Configure the EIC block to generate an interrupt every time the user presses the switch SW0 as shown in the accompanying image, and enable debounce functionality to avoid debouncing on the switch pin.

Configure LED Pin
Select the MPLAB® Code Configurator (MCC) Pin Settings tab and then scroll down to 21 in the Pin Number column and configure the PORT pin PC05 as an output pin for LED functionality as shown in the accompanying image.

Rename the default main file
Under the Project Graph tab, click on System and configure as shown to give a name of your liking to the default template main file generated by MCC.