Getting Started with MPLAB® Harmony v3 Drivers on SAM D21 MCUs Using FreeRTOS™: Step 1
Create MPLAB® Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.

In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

Browse to the folder you downloaded the framework to in the Framework Path edit box. Then click Next.
- The path to your MPLAB Harmony 3 installation folder should already be populated. if not, create a folder somewhere on your computer, like C:\harmony3, and point the project to that path.
- The MPLAB Harmony 3 necessary files will be downloaded to that path later during these steps.

In the Project Settings window, apply the following settings:
- Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\harmony_projects.
- Folder: Indicates the name of the MPLABX.X folder. Enter "drivers_freertos_sam_d21_xpro" to create a drivers_freertos_sam_d21_xpro.X folder.
This must be a valid directory name for your operating system.
- Name: Enter the project’s logical name as "getting_started_drivers_freertos_sam_d21_xpro". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to Configuration Settings.


Follow the steps below to set the project’s Configuration Settings.
- Name: Enter the configuration name as "sam_d21_xpro".
- Target Device: Select ATSAMD21J18A as the target device.
After selecting the target device, click Finish to launch the MCC.

The MCC Content Manager window is displayed. In this click Select MPLAB Harmony (by default this option is selected).

Click Launch to launch the MCC tool with the packages.

The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right click on the project name getting_started_drivers_freertos_sam_d21_xpro. Go to Set Configuration and select Customize....

Select SAM D21 Xplained Pro as the Connected Hardware Tool. Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in the MPLAB X IDE and then selecting Plugins > Clock Configuration.

A new window, Clock Easy View, is opened inside MCC.
In the Clock Easy View window, verify that the Main Clock is set to 48 MHz.