MPLAB® Harmony v3 Peripheral Libraries on SAM D21: Step 1
Create a project and configure the SAM D21
Install the MPLAB® Code Configurator (MCC) Plugin in the MPLAB X IDE or verify that MCC is installed.
• Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB® Code Configurator in the menu. If you don't see it in the menu, please install MCC.

Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework to, then click Next.

In the Project Settings window, apply the following settings:
- Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLAB X IDE .X folder. Enter "sam_d21_xpro" to create a sam_d21_xpro.X folder.
- Name: Enter the project’s logical name as "getting_started_sam_d21_xpro". This is the name that will be shown within the MPLAB X IDE.
- Click Next to proceed to configuration settings.


Follow the steps below to set the project’s configuration settings:
- Name: enter the configuration name as "sam_d21_xpro".
- Target Device: select ATSAMD21J18A as the target device.
- After selecting the target device, click Finish to launch MCC.

While the MCC tool launches, Click on Select MPLAB Harmony content type.

Click on the Finish button in the MCC Content Manager Wizard.

The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane in MPLAB X IDE. Right click on the project name getting_started_sam_d21_xpro and go to Set Configuration > Customize.

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to Project Graph in MPLABX IDE and then select Plugins > Clock Configuration.

A new window, Clock Easy View is opened inside MCC.
In the Clock Easy View, verify that the Main Clock is set to 48 MHz.