MPLAB® Harmony v3 Drivers on SAM E54 MCUs Using FreeRTOS™: Step 2
Configure I2C Driver and I2C Pins
Under the Available Components tab, expand Harmony > Drivers > I2C.
- Select and double-click on I2C to add the Inter-Integrated Circuit (I2C) driver to the project.




Select FreeRTOS and view the Configuration Options on the right. Depending on the requirements of the application, the FreeRTOS default configuration can be changed using the Graphical User Interface (GUI). For this tutorial, you will use the default configuration.

- Associate I²C driver with I²C instance 0 (SERCOM3) peripheral by right-clicking on the red diamond.


- Click on Instance 0 under I²C Driver to view the Configuration Options. Change the Number of Clients to 2.


Click on I²C to verify the driver is configured in Synchronous mode.

- Select SERCOM3 Peripheral Library and notice the default configuration by expanding Hardware Settings.

Open the Pin Configuration tabs by clicking Project Graph > Plugins > Pin Configuration.

Select the Pin Settings tab and sort the entries by Ports as shown:

Now, select the Pin Table tab and then scroll down to the SERCOM3 module as shown:
- Enable I²C Clock (SCL) (SERCOM3_PAD1) on PA23 (Pin #93).
- Enable I²C Data (SDA) (SERCOM3_PAD0) on PA22 (Pin #92).

This completes the configuration of the I2C driver. The application code will use the I²C driver APIs to read the temperature from the temperature sensor and store it in EEPROM. The application also retrieves the last five temperature values stored in the EEPROM.
Configure Universal Synchronous Asynchronous Receiver Transmitter (USART) Driver and USART Pins
Under the Device Resources tab, expand Harmony > Drivers > SQI Flash > USART.
- Double-click on USART to add the Universal Synchronous Asynchronous Receiver Transmitter (USART) driver to the project.


- Associate USART Driver with USART instance 1 (SERCOM2) peripheral by right-clicking on the red diamond.


- Verify USART driver is configured to run in Synchronous mode by clicking on the USART block as shown:

- Click on Instance 0 under USART Driver to view the Configuration Options. Change the number of clients to the USART driver Instance from 0 to 3. The User Input Thread will use the USART driver to read the character input on the serial terminal. The Sensor and EEPROM threads will use the USART driver to print temperature values on the serial terminal.

- Select the SERCOM2 Peripheral Library in the Project Graph and configure it for USART protocol, including setting the Baud rate to 115,200 Hz.

Select the Pin Table tab and then scroll down to the SERCOM2 module as shown:
- Enable USART_RX on PB24 (Pin #100).
- Enable USART_TX on PB25 (pin #101).