MPLAB® Harmony v3 Peripheral Libraries on SAM D5x/E5x: Step 1
Install the MPLAB® Code Configurator (MCC) Plug-in in the MPLAB X IDE
Verify that MCC is installed
Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
Go to Tools > Embedded.
You will see MPLAB Code Configurator in the menu.

If you don't see it in the menu, install MHC.
Create MPLAB Harmony v3 Project using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework to. If you haven't done this, or want to download it to a different folder, click the Launch Framework Downloader button, then click Next.

In the Project Settings window, apply the following settings:
Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLABX .X folder. Enter "sam_e54_xpro" to create a sam_e54_xpro.X folder.
- Name: enter the project’s logical name as "getting_started_sam_e54_xpro". This is the name that will be shown from within the MPLAB X IDE.
Click Next to proceed to configuration settings.


Follow the steps below to set the project’s Configuration Settings:
Name: enter the configuration name as "sam_e54_xpro".
- Target Device: select ATSAME54P20A as the target device.
After selecting the target device, click Finish to launch the MCC.

While the MCC tool launches, click on Select MPLAB Harmony content type

Click on the Finish button in the MCC Content Manager Wizard.

The MCC plugin’s main window for the project will be displayed.
Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right click on the project name getting_started_sam_C1n_xpro and go to Set Configuration > Customize.

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Select Simulator for Hardware Toolchain. Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to Project Graph in MPLAB X IDE and then select Plugins > Clock Configuration.

A new window, Clock Easy View, is opened in the project’s main window.
Click on the Clock Easy View tab, scroll to the right and verify that the Main Clock is set to 120 MHz.