Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
MPLAB® Harmony v3 Peripheral Libraries on SAM D5x/E5x: Step 3
Last modified by Microchip on 2023/11/09 09:09
Configure Switch Button Pin to Generate an Interrupt
In the MPLAB® Code Configurator (MCC), select the Pin Settings tab and then scroll down to 122 in the Pin Number column and configure the PORT pin PB31 as an external interrupt pin for switch functionality as shown in the accompanying image. The internal pull-up is enabled to avoid false edge detection as there is no external pull-up on the SAM E54 Xplained Pro Evaluation Kit.
Select the Project Graph tab.
Add the External Interrupt Controller (EIC) to the project.
Under the left side tab, Resource Management (MCC), go to Device Resources and expand Libraries > Harmony > Peripheral > EIC. Select and double click on EIC to add the EIC module to the project.
Configure the EIC block to generate an interrupt every time the user presses the switch SW0 as shown in the accompanying image, and enable debounce functionality to avoid debouncing on switch pin.
Select the MCC Pin Settings tab and then scroll down to 72 in the Pin Number column and configure the PORT pin PC18 as an output pin for LED functionality as shown in the accompanying image.
Information
Note: The LED on the SAM E54 Xplained Pro board is active low. Configure the LED in the default OFF state by configuring the latch value to logic "High".
Under the Project Graph tab, click on System, and configure as it to give a name of your liking to the default template main file generated by the MCC.
Information
Note: The name of the default main.c is changed to main_e54.c to indicate that the referred main.c is for the SAM D5x/E5x getting started training module.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.