MPLAB® Harmony v3 Drivers on SAM E70/S70/V70/V71 Using FreeRTOS™: Step 1
Install MPLAB® Code Configurator (MCC) Plugin in MPLAB X IDE
Verify that MPLAB Code Configurator (MCC) is installed.
• Launch MPLAB X IDE from the Windows® Start menu. Close any projects and files that are currently open.
• Go to Tools > Embedded.
• You will see MPLAB® Code Configurator v5: Open/Close in the menu.

If you don't see it in the menu, install MCC.
Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the main IDE menu.
In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

Browse to the folder you downloaded the framework to in the Framework Path edit box. Then click Next.
For more information on the framework downloader, see the "MPLAB® Code Configurator (MCC)" page.

In the Project Settings window, apply the following settings:
Location
Location indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev.
Folder
Folder indicates the name of the MPLABX .X folder. Enter "drivers_freertos_sam_e70_xult" to create a drivers_freertos_sam_e70_xult.X folder.
Name
Enter the project’s logical name as "getting_started_drivers_freertos_sam_e70_xult". This is the name that will be shown from within the MPLAB X IDE.
Click Next to proceed to Configuration Settings.


Follow the steps below to set the project’s Configuration Settings.
Name:
Enter the configuration name as "sam_e70_xult".
Target Device:
Select ATSAME70Q21B as the target device.
After selecting the target device, click Finish to launch the MCC.

The MCC content manager window is displayed. In this click Select MPLAB Harmony (by default this option is selected).

Click Finish to launch the MCC tool with the packages.

The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the Projects tab on the top left pane. Right-click on the project name getting_started_drivers_freertos_sam_e70_xult.
Go to Set Configuration and click on Customize...

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32 and select the Simulator.
Click on Apply and then OK.

Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in the MPLAB X IDE and then select Plugins > Clock Configuration.
A new window, Clock Diagram, is opened in the project’s main window.
Click on the Clock Diagram tab, scroll to the right and verify that the Processor Clock (HCLK) and Master Clock (MCK) are set to 300 MHz and 150 MHz, respectively.