MPLAB® Harmony v3 Drivers and System Services on SAM E70/S70/V70/V71: Step 3
Configure the LED pin.
In this step, the user LED on the SAM E70 Xplained Ultra Evaluation Kit will be configured according to the USER_LED design schematic.

Figure 1
In MPLAB® Code Configurator (MCC), select the Pin Settings tab, scroll down to PA5 (Pin Number 73) in the Pin ID column, and then configure the PORT pin PA5 as an output pin for LED functionality.

Figure 2
Rename the default main file.
Under the Project Graph tab, click on System and give a name of your liking to the default template main file generated by the MCC.

Figure 3
Configure Application Tasks.
Go to the Project Graph and select Harmony Core.

Figure 4
The Configuration Options show that for a Harmony project, MCC automatically enables the generation of application files (app.c and app.h).
Change the Number of Applications to 2.
Expand Application 0 Configuration and rename the default application name to app_sensor.
Expand Application 1 Configuration and rename the default application name to app_eeprom as shown in Figure 5. Press the Enter key to save the application name.

Figure 5